I'm just getting started with my new FRWY-LS1012a and followed some of the first instructions to reprogram uboot. After following the instructions in "Layerscape LS1012A Freeway (FRWY-LS1012A) Board Getting Started Guide, Rev. 1, 05/2018", section 4.4 Step 3: "Programming BSP composite firmware image", my board no longer boots. I'm mostly curious about what exactly when wrong here. Here is a transcript, which after a reset, the board is bricked:
=> tftp firmware_ls1012afrwy_uboot_qspiboot.img pfe_eth0 Waiting for PHY auto negotiation to complete......... TIMEOUT ! Could not initialize PHY pfe_eth0 Speed detected 3e8 Using pfe_eth1 device TFTP from server 192.168.8.8; our IP address is 192.168.8.111 Filename 'firmware_ls1012afrwy_uboot_qspiboot.img'. Load address: 0x0 Loading: ################################################################# ########################################## 3.1 MiB/s done Bytes transferred = 1557830 (17c546 hex) => sf probe 0:0;sf erase 0 +$filesize; sf write 96000000 0 $filesize SF: Detected w25q16dw with page size 256 Bytes, erase size 4 KiB, total 2 MiB SF: 1560576 bytes @ 0x0 Erased: OK device 0 offset 0x0, size 0x17c546 SF: 1557830 bytes @ 0x0 Written: OK => sf erase 0x1d0000 +0x10000; SF: 65536 bytes @ 0x1d0000 Erased: OK
The firmware was obtained via:
wget https://www.nxp.com/lgfiles/sdk/lsdk1712-ls1012afrwy/firmware_ls1012afrwy_uboot_qspiboot.img
Best,
Chris
Darn, it was my tftp load address. Makes sense.
I have the same problem, any solution?