CCSR Block Address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCSR Block Address

1,798件の閲覧回数
rashmikj
Contributor III

Hi,

The CCSR Block_Base_Address starts from 1000000...Why are we excluding 1 in rcw files?? like for ex in file rcw_1200_qspiboot.rcw , it is written as write 0x57015c, 0x40100000??

ラベル(1)
0 件の賞賛
返信
1 返信

1,746件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1021A Reference Manual, Table 9-2. Required format of data structure used by PBL, note 2:

"SYS_ADDR = 0x61_0040 is a PBI CRC check command (PBL block base address 0x161_0000, but only 24-bits address are used here)."

Also consider that "write" in PBI corresponds to the ACS=0 (CCSR space) and "awrite" corresponds to the ACS=1.

0 件の賞賛
返信