Boot LS 1012A (FRDM) from USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot LS 1012A (FRDM) from USB

4,069 Views
pieterdewachter
Contributor I

I have currently compiled the QorIQ SDK (update 1703) for the (LS1012A FRDM) board, more specifically fsl-image-full and fsl-image-kernelitb. This gives me some u-boot, rcw, kernel and rootfs files / images. Now I would like to boot this extended Linux (the full image) from a USB drive. Unfortunately I'm not sure as of how to setup the environment correctly to achieve this.

The USB drive is recognized correctly in both the U-boot bootloader and the Linux that came preinstalled on the board. Some debug info:

     => usb storage
     Device 0: Vendor: Intenso Rev: 1.00 Prod: Speed Line
     Type: Removable Hard Disk
     Capacity: 15237.1 MB = 14.8 GB (31205621 x 512)


     => usb part

     Partition Map for USB device 0 -- Partition Type: DOS

     Part Start Sector Num Sectors UUID Type
     1 32 31205344 0005d59e-01 83

     => usb dev

     USB device 0: Vendor: Intenso Rev: 1.00 Prod: Speed Line
     Type: Removable Hard Disk
     Capacity: 15237.1 MB = 14.8 GB (31205621 x 512)

The drive has been formatted as ext2 and I put all the files of the rootfs archive (extracted it) and the kernel-fsl-ls1012a-frdm.itb file on it.

Thanks in advance!

Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

3,397 Views
zmlopez
Contributor III

I've already done it, but with dtb and kernel files instead of itb:

(I'm using OpenWRT distribution instead of Yocto)

Two partitions in the usb drive, made with gparted in linux.

First one, a small FAT partition, second an ext4 file system.

In the first one, I've put the following files:

image-fsl-ls1012a-frdm.dtb

ls1012afrdm-kernel.bin

In the second partition, the linux file system.

Uboot commands:

usb start
fatload usb 0:1 90000000 image-fsl-ls1012a-frdm.dtb

fatload usb 0:1 96000000 ls1012afrdm-kernel.bin
setenv bootargs "console=${console},${baudrate} root=/dev/sda2 rootwait rw"
bootm 96000000 - 90000000

In your case, this should work, if the itb file is in root of usb drive:

usb start
ext2load usb 0:1 90000000 kernel-fsl-ls1012a-frdm.itb
setenv bootargs "console=${console},${baudrate} root=/dev/sda1 rootwait rw"
bootm 90000000

Hope this helps.

0 Kudos
Reply

3,397 Views
pieterdewachter
Contributor I

I tried to follow these steps, but it seems like I am missing some files to do so correctly. I only have an image .bin file so I used that one instead, without luck unfortunately. The files I have are listed on this screenshot:screenshot.png

0 Kudos
Reply

3,397 Views
zmlopez
Contributor III

You need uImage format, not Image, to load it with bootm in u-boot (or zImage if you use bootz).

uImage has a wrapper to tell u-boot how to load the binary file, created with mkimage.

Have you tried with the itb file?

usb start
ext2load usb 0:1 90000000 kernel-fsl-ls1012a-frdm.itb
setenv bootargs "console=${console},${baudrate} root=/dev/sda1 rootwait rw"
bootm 90000000

I can't test it myself rigth now, because I don't have an itb file generated in my system.

0 Kudos
Reply

3,397 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 4.4.9.5.3 of SDK 2.0-1703 documentation about "Deploying the full file system":

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,397 Views
pieterdewachter
Contributor I

Thank you for the advice, unfortunately I keep getting this message when performing the steps described in that section:

   ERROR: can't get kernel image!

0 Kudos
Reply