Any PBL tutorial?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Any PBL tutorial?

4,125 次查看
bladerunner1010
Contributor III

??

 

0 项奖励
回复
7 回复数

4,120 次查看
ufedor
NXP Employee
NXP Employee

1) Recommended way is to use CodeWarrior QCVS PBL Tool:

https://www.nxp.com/docs/en/user-guide/QCVS_PBL_User_Guide.pdf

2) You wrote:

> from external DSPI NOR Flash

What do you mean?

 

 

0 项奖励
回复

4,117 次查看
bladerunner1010
Contributor III

??

0 项奖励
回复

4,112 次查看
ufedor
NXP Employee
NXP Employee

> The device will boot from external flash using DSPI interface.

Excuse me, where this interface is shown in the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings?

0 项奖励
回复

4,057 次查看
bladerunner1010
Contributor III

Which changes are required?

0 项奖励
回复

4,053 次查看
ufedor
NXP Employee
NXP Employee

> Is it possible to boot from DSPI with LS1023?

All possible boot sources are specified in the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings.

4,043 次查看
bladerunner1010
Contributor III

??

 

0 项奖励
回复

4,036 次查看
ufedor
NXP Employee
NXP Employee

The question is not clear.

It is possible to refer to the LS1043ARDB RCW sources at:

https://source.codeaurora.org/external/qoriq/qoriq-components/rcw/tree/ls1043ardb/RR_FQPP_1455?h=LSD...

0 项奖励
回复