Any PBL tutorial?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any PBL tutorial?

4,053件の閲覧回数
bladerunner1010
Contributor III

??

 

0 件の賞賛
返信
7 返答(返信)

4,048件の閲覧回数
ufedor
NXP Employee
NXP Employee

1) Recommended way is to use CodeWarrior QCVS PBL Tool:

https://www.nxp.com/docs/en/user-guide/QCVS_PBL_User_Guide.pdf

2) You wrote:

> from external DSPI NOR Flash

What do you mean?

 

 

0 件の賞賛
返信

4,045件の閲覧回数
bladerunner1010
Contributor III

??

0 件の賞賛
返信

4,040件の閲覧回数
ufedor
NXP Employee
NXP Employee

> The device will boot from external flash using DSPI interface.

Excuse me, where this interface is shown in the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings?

0 件の賞賛
返信

3,985件の閲覧回数
bladerunner1010
Contributor III

Which changes are required?

0 件の賞賛
返信

3,981件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is it possible to boot from DSPI with LS1023?

All possible boot sources are specified in the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings.

3,971件の閲覧回数
bladerunner1010
Contributor III

??

 

0 件の賞賛
返信

3,964件の閲覧回数
ufedor
NXP Employee
NXP Employee

The question is not clear.

It is possible to refer to the LS1043ARDB RCW sources at:

https://source.codeaurora.org/external/qoriq/qoriq-components/rcw/tree/ls1043ardb/RR_FQPP_1455?h=LSD...

0 件の賞賛
返信