Layerscape知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Layerscape Knowledge Base

讨论

排序依据:
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images on the SD card.    Compiling MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/ls1088a/ $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-18.09 The prebuilt MC firmware image, mc_10.10.0_ls1088a_20180814.itb, is available at qoriq-mc-binary/ls1088a/. Note that the exact name of the MC firmware image may vary depending on the release version used.                  Compiling DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils/ $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-18.09 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc.0x1D-0x0D.dtb and dpl-eth.0x1D_0x0D.dtb images are available at /mc-utils/config/ls1088a/RDB/. Note that the exact name of the DPL and DPC images may vary depending on the release version used.             SD card start block number for MC, DPL, and DPC images Image  SD card start block number DPAA2 MC firmware 0x05000 = 20480 DPAA2 DPL  0x06800 = 26624 DPAA2 DPC 0x07000 = 28672 Refer the Layerscape Software Development Kit <version> Documentation for complete listing of the SD card start block numbers for all LSDK firmware images.    Programming MC, DPC, and DPL images to SD card Plug the SD card into the Linux host. Run the following commands on the Linux host: To update MC firmware: $ sudo dd if=mc_10.10.0_ls1088a_20180814.itb of=/dev/sdX bs=512 seek=20480 conv=fsync To update DPL image: $ sudo dd if=dpl-eth.0x1D_0x0D.dtb of=/dev/sdX bs=512 seek=26624 conv=fsync To update DPC image: $ sudo dd if=dpc.0x1D-0x0D.dtb of=/dev/sdX bs=512 seek=28672 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically  mmcblk0.   Remove the SD card from the Linux host machine. On the LS1088ARDB/LS1088ARDB-PB, ensure that the switches are set to boot the board from the SD card.  For booting from SD card, SW1[1:8] + SW2[1] = 0010_0000_0  Plug the SD card into the board and boot the board to Ubuntu. If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
查看全文
This how-to topic is applicable only to LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries on SD card. Follow these steps to update U-Boot binary on the SD card.  Prerequisites  Ubuntu 18.04 64-bit should be installed on the Linux host machine for building LSDK 18.06 or LSDK 18.09 U-Boot binary.   Compiling U-Boot binary Clone the u-boot repository. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean Execute appropriate defconfig file: For LS1088ARDB: $ make ls1088ardb_sdcard_qspi_defconfig For LS1088ARDB-PB: $ make ls1088ardb_pb_sdcard_qspi_defconfig If required, make changes to the U-Boot files. $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.06 or LSDK 18.09 U-Boot binary.  The compiled U-Boot image, u-boot-with-spl.bin, is available at u-boot/. SD card start block number for U-Boot binary Image  SD card start block number U-Boot binary 0x00800 = 2048 Refer the Flash layout for boot flow with PPA – LSDK 18.09 and older releases for a complete listing of the SD card start block numbers for all LSDK firmware images.     Programming U-Boot binary to SD card Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=u-boot-with-spl.bin of=/dev/sdX bs=512 seek=2048 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/ sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.    Remove the SD card from the Linux host machine. On the LS1088ARDB/LS1088ARDB-PB, ensure that the switches are set to boot the board from SD card.  For booting from SD card, SW1[1:8] + SW2[1] = 0010_0000_0  Plug the SD card into the board and boot the board to Ubuntu. If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
查看全文
Follow these steps to update the composite firmware image in QSPI NOR flash. cpld reset boots the board from QSPI NOR flash0 and cpld reset altbank boots the board from QSPI NOR flash1. sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1. Obtaining composite firmware image  LSDK includes pre-built firmware images for QSPI NOR flash. The LSDK composite firmware includes RCW+PBI, U-Boot/UEFI, PPA, boot loader environment variables, DPAA1 FMan ucode, QE/uQE firmware, Ethernet PHY firmware, device tree, and lsdk_linux_<arch>.itb images. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout of the images.  On a Linux host machine, download composite firmware image for QSPI boot from nxp.com.    $ wget http://www.nxp.com/lgfiles/sdk/lsdk<LSDK version>/firmware_<RDB_name>_uboot_qspiboot.img    For example:  $ wget http://www.nxp.com/lgfiles/sdk/lsdk1812/firmware_ls1046ardb_uboot_qspiboot.img  Flashing composite firmware images to QSPI NOR flash Composite firmware image can be loaded to LS1046ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Boot LS1046RDB from QSPI NOR flash. Ensure that the switches are set to boot the board from QSPI NOR flash. For booting from QSPI flash, SW5[1:8] = 00100010 Boot from QSPI NOR flash0: => cpld reset In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1, FM1@TGEC2 Set server IP to the IP of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. Refer LS1046ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime FM1@DTSEC4 => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact FM1@DTSEC4 Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command. Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using FM1@DTSEC4 device host 192.168.1.1 is alive   Load composite firmware image from the TFTP server Program QSPI NOR flash1: => sf probe 0:1 Flash composite firmware image: => tftp a0000000 firmware_ls1046ardb_uboot_qspiboot.img => print filesize filesize=2351db0 Program composite firmware image to QSPI NOR flash: => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Address 0x0 is the location of the composite firmware image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1: => cpld reset altbank In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 4 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash. Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Boot LS1046RDB from QSPI NOR flash. Ensure that the switches are set to boot the board from QSPI NOR flash. For booting from QSPI flash, SW5[1:8] = 00100010 Boot from QSPI NOR flash0: => cpld reset In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 0 Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 Program QSPI NOR flash1: => sf probe 0:1 Load composite firmware image from the storage device => load mmc 0:2 a0000000 <image name> => print filesize For example: => load mmc 0:2 a0000000 firmware_ls1046ardb_uboot_qspiboot.img => print filesize filesize=2351db0 Or => load usb 0:2 a0000000 <image name> => print filesize Or => load scsi 0:2 a0000000 <image name> => print filesize If the ls command fails to run, check that U-Boot in QSPI NOR flash0 supports the command by typing ls at the U-Boot prompt: => ls ls - lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in QSPI NOR flash0. Program image to QSPI NOR flash: => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize Address  0x0 is the location of the composite firmware image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout.  Boot from QSPI NOR flash1: => cpld reset altbank In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 4 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.
查看全文
The table below shows the mapping of the Ethernet port names appearing on the front panel of the LS1043ARDB chassis with the port names in U-Boot, tinyDistro, and NXP LSDK userland.  Ethernet port mapping Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro) Port name in Linux (LSDK userland) QSGMII.P0 FM1@DTSEC1 eth0 fm1-mac1 QSGMII.P1 FM1@DTSEC2 eth1 fm1-mac2 QSGMII.P2 FM1@DTSEC3 eth2 fm1-mac5 QSGMII.P3 FM1@DTSEC4 eth3 fm1-mac6 RGMII1 FM1@DTSEC5 eth4 fm1-mac3 RGMII2 FM1@DTSEC6 eth5 fm1-mac4 10G Copper FM1@TGEC1 eth6 fm1-mac9 Below is a table that shows the mapping between port numbers (from configuration file), character devices, hardware ports (Rx) and mEMACs for the standard SDK configuration (using RCW protocol 1455). FMC port mapping Port name on chassis XML port number (configuration file) Serdes protocol Character device Hardware port (device tree node) mEMAC (device tree node) QSGMII.P0 1 qsgmii fm0-port-rx0 port@88000 ethernet@e0000 QSGMII.P1 2 qsgmii fm0-port-rx1 port@89000 ethernet@e2000 QSGMII.P2 5 qsgmii fm0-port-rx4 port@8c000 ethernet@e8000 QSGMII.P3 6 qsgmii fm0-port-rx5 port@8d000 ethernet@ea000 RGMII1 3 rgmii fm0-port-rx2 port@8a000 ethernet@e4000 RGMII2 4 rgmii fm0-port-rx3 port@8b000 ethernet@e6000 10G Copper 9 xgmii fm0-port-rx6 port@90000 ethernet@f0000
查看全文
This document introduces porting TDM Linux driver working in internal loopback mode to do verification during custom boards bringing up and verification stage. 1. TDM Interface Configuration to Support Internal Loopback Mode 2. Modify Linux Kernel Driver to Make TDM Working in Internal Loopback Mode 3. Build TDM Driver into Linux Kernel and do verification on the target board
查看全文
The table below shows the mapping of the Ethernet port names appearing on the front panel of the LS1046ARDB chassis with the port names in U-Boot, tinyDistro, and NXP LSDK userland.  Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro) Port name in Linux (LSDK userland) RGMII1 FM1@DTSEC3 eth0 fm1-mac3 RGMII2 FM1@DTSEC4 eth1 fm1-mac4 SGMII1 FM1@DTSEC5 eth2 fm1-mac5 SGMII2 FM1@DTSEC6 eth3 fm1-mac6 10G Copper FM1@TGEC1 eth4 fm1-mac9 10G SEP+ FM1@TGEC2 eth5 fm1-mac10
查看全文
The attached patch is to support Aquantia AQR107 in LS1043A.
查看全文
  ARM Cortex A57 and A53 L1/L2 cache error reporting    The attached patch adds error detection for A53 and A57 cores. Hardware error injection is supported on A53. Software error injection is supported on both. For hardware error injection on A53 to work, proper access to L2ACTLR_EL1, CPUACTLR_EL1 needs to be granted by EL3 firmware. This is done by making an SMC call in the driver. Failure to enable access disables hardware error injection. For error interrupt to work, another SMC call enables access to L2ECTLR_EL1. Failure to enable access disables interrupt for error reporting. CPU Memory Error Syndrome and L2 Memory Error Syndrome registers can be used for checking L1 and L2 memory errors. However, only A53 supports double-bit error injection to L1 and L2 memory. This driver uses the hardware error injection when available, but also provides a way to inject errors by software. Both A53 and A57 supports interrupt when multi-bit errors happen. To use hardware error injection and the interrupt, proper access needs to be granted in ACTLR_EL3 (and/or ACTLR_EL2) register by EL3 firmware SMC call. Correctable errors do not trigger such interrupt. This driver uses dynamic polling internal to check for errors. The more errors detected, the more frequently it polls. Combining with interrupt, this driver can detect correctable and uncorrectable errors. However, if the uncorrectable errors cause system abort exception, this driver is not able to report errors in time.    Build ATF and Kernel image with EDAC L1 and L2 cache error detection enabled in LSDK In LLDPUG_RevL6.1.22_2.0.0 Yocto build environment, please rebuild ATF as the following. $ source build_ls1043ardb/SOURCE_THIS $ bitbake qoriq-atf -c cleansstate $ bitbake qoriq-atf -c patch Please go to atf source code folder build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/qoriq-atf/2.8+AUTOINC+atf-r0/git/, please apply patch 0001-Porting-helper-functions-for-EDAC-support-based-on-L.patch. $ patch -p1 < 0001-Porting-helper-functions-for-EDAC-support-based-on-L.patch And rebuild atf image. $ bitbake qoriq-atf Please rebuild Linux Kernel with the following commands. $ source build_ls1043ardb/SOURCE_THIS $ bitbake virtual/kernel -c cleansstate $ bitbake virtual/kernel -c patch Please go to Linux Kernel source code folder build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/git/ to apply patch 0001-drivers-edac-Add-L1-and-L2-error-detection-for-A53-a.patch. $ patch -p1 < 0001-drivers-edac-Add-L1-and-L2-error-detection-for-A53-a.patch   $ bitbake virtual/kernel -c menuconfig yipingwang_0-1783326465815.png   $ bitbake virtual/kernel   L1/L2 cache error detection and correction EDAC feature verification root@localhost:~# dmesg | grep edac [ 3.478641] EDAC DEVICE0: Giving out device to module edac-a53 controller cortex_edac_l1_l2: DEV edac-a53 (POLLED) root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l1_ue_sw_inject root@localhost:~# [ 74.784912] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 0 [ 74.784912] ' root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l1_ue_hw_inject [ 83.429371] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 3 [ 83.429371] ' root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l2_ue_sw_inject root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l2_ue_hw_inject [ 106.985393] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0 [ 106.985393] ' [ 106.997164] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 1 [ 106.997164] ' root@localhost:~# [ 115.232986] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0 [ 115.232986] ' root@localhost:~# dmesg | grep EDAC [ 1.638675] EDAC MC: Ver: 3.0.0 [ 3.478641] EDAC DEVICE0: Giving out device to module edac-a53 controller cortex_edac_l1_l2: DEV edac-a53 (POLLED) [ 74.784840] EDAC cortex_edac_l1_l2: CPU 0 L1-I Tag RAM error(s) detected [ 74.784869] EDAC cortex_edac_l1_l2: CPU 0 L1 fatal error(s) detected (0x8000000080000000) [ 74.784912] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 0 [ 83.429298] EDAC cortex_edac_l1_l2: CPU 3 L1-D Data RAM error(s) detected [ 83.429329] EDAC cortex_edac_l1_l2: CPU 3 L1 fatal error(s) detected (0x8000000089100010) [ 83.429371] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 3 [ 106.985331] EDAC cortex_edac_l1_l2: CPU 0 L2 fatal error(s) detected (0x80000000910dc138) [ 106.985349] EDAC cortex_edac_l1_l2: CPU 1 L2 fatal error(s) detected (0x8000000080000000) [ 106.985393] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0 [ 106.997164] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 1 [ 115.232936] EDAC cortex_edac_l1_l2: CPU 0 L2 fatal error(s) detected (0x80000000910c0598) [ 115.232986] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0  
查看全文
Introduction The qDMA controller transfers blocks of data between one source and one destination. The blocks of data transferred can be represented in memory as contiguous or noncontiguous using scatter/gather table(s). Channel virtualization is supported through enqueuing of DMA jobs to, or dequeuing DMA jobs from, different work queues. QDMA can support LX2160A with DPAA2. The attached patch is used for QDMA data transfer between PCIe Endpoint and DDR memory on LX2160A Platform. Apply the patch and rebuild Kernel image in LSDK 21.08 Go to LSDK 21.08 Linux Kernel source folder components/linux/linux/   Apply the attached patch. $ patch -p1 < 0001-QDMA-Performance-test.patch   $ flex-builder -c linux:custom -a arm64 Enable CONFIG_FSL_DPAA2_QDMA=y   $ Rebuild Linux Kernel. $ flex-builder -c linux -a arm64   Transfer data from Memory to Memory root@localhost:~# restool dpdmai create --num-queues=8 --priorities=2,5 dpdmai.0 is created under dprc.1 root@localhost:~# restool dprc assign dprc.1 --object=dpdmai.0 --plugged=1 root@localhost:~# echo "dpdmai.0" > /sys/module/dmatest/parameters/device root@localhost:~# echo '7       4       1       7' > /proc/sys/kernel/printk root@localhost:~# echo 1 > /sys/module/dmatest/parameters/dmatest_option root@localhost:~# echo 10 > /sys/module/dmatest/parameters/iterations root@localhost:~# echo 4096 > /sys/module/dmatest/parameters/test_buf_size root@localhost:~# echo 1 > /sys/module/dmatest/parameters/threads_per_chan root@localhost:~# echo 1 > /sys/module/dmatest/parameters/run [  177.903819] dmatest: current_mask 1 root@localhost:~# [  177.907636] dmatest: len 11         save_mask ffff  tmp_mask 2 [  178.927396] dmatest: qdma-test-task: summary 10 tests, 0 failures 303030 iops 1212121 KB/s 1241212121 B/s (0) [  178.937308] dmatest: total_len 40960  len 4096 [  178.941870] dmatest: runtime 33 [  178.941870]   root@localhost:~# echo 8 > /sys/module/dmatest/parameters/threads_per_chan root@localhost:~# echo 1 > /sys/module/dmatest/parameters/run [  273.731698] dmatest: current_mask 1 root@localhost:~# [  273.735625] dmatest: len 11         save_mask ffff  tmp_mask 2 [  274.767409] dmatest: qdma-test-task: summary 10 tests, 0 failures 357142 iops 1428571 KB/s 1462857142 B/s (0) [  274.777315] dmatest: total_len 40960  len 4096 [  274.781875] dmatest: runtime 28 [  274.781875]   Transfer data from Memory to PCIe  root@lx2160ardb-rev2:~# restool dpdmai create --num-queues=8 --priorities=2,5 dpdmai.0 is created under dprc.1 root@lx2160ardb-rev2:~# restool dprc assign dprc.1 --object=dpdmai.0 --plugged=1 root@lx2160ardb-rev2:~# echo "dpdmai.0" > /sys/module/dmatest/parameters/device root@lx2160ardb-rev2:~# echo '7       4       1       7' > /proc/sys/kernel/printk root@lx2160ardb-rev2:~# echo 4096 > /sys/module/dmatest/parameters/test_buf_size root@lx2160ardb-rev2:~#  echo 10 > /sys/module/dmatest/parameters/iterations root@lx2160ardb-rev2:~# echo 2 > /sys/module/dmatest/parameters/dmatest_option root@lx2160ardb-rev2:~# echo 0x9040000000 > /sys/module/dmatest/parameters/pci_phys_addr root@lx2160ardb-rev2:~# echo 1 > /sys/module/dmatest/parameters/produ_task_number root@lx2160ardb-rev2:~# echo 1 > /sys/module/dmatest/parameters/run [  214.319248] dmatest: current_mask 1 root@lx2160ardb-rev2:~# [  214.322864] dmatest: len 11   save_mask ffff  tmp_mask 2 [  214.330187] dmatest: pcie_phy_base : 9040000000       pcie_virt_base : 0000000014415a49 [  215.355448] dmatest: qdma-test-task: summary 10 tests, 0 failures 26737 iops 106951 KB/s 109518716 B/s (0) [  215.365093] dmatest: total_len 40960  len 4096 [  215.369529] dmatest: runtime 374 [  215.369529]  
查看全文
The document explains how to use the variable  APTGET_EXTRA_PACKAGES in Yocto-based LLDP builds (ls-image-main.bb recipe) to install Ubuntu packages via apt-get instead of BitBake recipes.  
查看全文
When customer’s ethernet PCS could not link up, this article will give a guide how to debug it step by step based on the T1024. Many ethernet is configured by the SerDes, so how to confirm the link error is caused by the SerDes or the PCS itself. This article will give some clues. Serdes Lane&pins First check which SerDes lane the you are using, please confirm the SerDes land in the QorIQ T1024 Reference Manual. Such as configuration below, the user case set the SRDS_PRCTL_S1=0x05B in the RCW[128:136], the application will utilize the SGMII.m1 and SGMII.m2. 01.png fmacaddress.png This article will consider SGMII.m1 as an user case, now the SGMII will in the Frame Manager, MAC1. Check the SerDes Lane Assignments to confirm the Lane of the SerDes, for the SGMII.m1, the specific lane pins name would be SD1_TX3P/N and SD1_RX3P/N. it could be recognized as Lane 3. MAC number is not related to the Serdes lane number, should confirm the specific table to get the pins. lane.png Any hardware test with this ethernet should related the pins, see the component pin number below. pins.png You could test the eye diagram of RX pins of this Lane to confirm if the frequency is correct. if you set this Lane to SGMII 1.25G, you could confirm the speed is set correctly by the eye diagram. eyediagram.png Eye diagram above, just show the speed of the SerDes. That is very important when loopback correctly, but could to connect to other device. How to confirm the SerDes link up Please find the Lane register in the QorIQ T1024 Reference Manual. In this user case it’s Lane 3, so should read out the Lane 3 registers to confirm if the SerDes Lane 3 work well. Such as below: # Lane 3 md.l 0xFFE0EA8C0 1 - aa611080 # LN3GCR0 md.l 0xFFE0EA8C4 1 - 101c4019 # LN3GCR1 md.l 0xFFE0EA8CC 1 - 00002800 # LN3SSCR0 md.l 0xFFE0EA8D0 1 - 0f0fc01f # LN3RECR0 md.l 0xFFE0EA8D4 1 - 0f0f0fa8 # LN3RECR1 md.l 0xFFE0EA8D8 1 - 00003006 # LN3TECR0 md.l 0xFFE0EA8E0 1 - 39000400 # LN3TTLCR0 md.l 0xFFE0EA8E4 1 - 00000000 # LN3TTLCR1 md.l 0xFFE0EA8F4 1 - 00000000 # LN3TCSR1 md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3   SerDes_LNnTCSR3 is an important debug test register, the CDR_LCK is to check if the CDR locked or not. CDR_LCK=0 means a valid bit stream is not detected. As a test, you could put the lane in loopback mode LN2TCSR3[LPBK_EN]=01. The CDR should lock in digital loopback mode (internal loopback). If not, there could be an issue with the device itself. So, if you could set the LPBK-EN to “01” Loopback Mode, it will set the SerDes’s own TX and RX signals in Loopback Mode to exclude external signals, then check the CDR_LCK again, if it’s 1, then SerDes itself works well. Anyway, CDR_LCK should always be set. In the “md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3”, the CDR_LCK=0, suspect the SerDes level issue. The normal status should be: => md fe0ea8fc 1 fe0ea8fc: 08000000 CDR.png How to confirm the PCS link up The MAC and PHY registers should get the details from the T1024DPAArm, QorIQ T1024 Data Path Acceleration Architecture (DPAA) Reference Manual Find the offset address in the DPAARM. FMAC2.png For the SGMII MAC address should be offset+0x1000. Follow the 6.5.4 MDIO Ethernet Management Interface usage in the T1024DPAARM to read the MDIO registers. In this application, SGMII1, MAC1, you could find the MAC1 address would be FM1_mEMAC1: 4E_0000, so FM1_mEMAC1 MDIO registers would be 4E_1000h. In the user case, the protocol is SGMII, should follow the 6.5.4.3 Clause 22 Read Flow in the T1024DPAARM. 6.5.4.3 Clause 22 Read Flow 1) Wait for MDIO_CFG[BSY] = 0. 2) Write MDIO_CTL with proper PHY_ADDR and REGISTER_ADDR and with bit 16 set. 3) Wait for MDIO_CFG[BSY] = 0. 4) If the addressed PHY did not respond then MDIO_CFG[MDIO_RD_ER] is set. Otherwise read MDIO_DATA value. In this user case, should read the MDIO_SGMII_SR, you could find the register definition in the QorIQ T1024 Reference Manual, 30.5.5 1000Base-KX PCS MDIO Memory Map/Register Definition The key bits would below: STATUSREG.png STATUSREG2.png Here the user case result: When you read MDIO_SGMII_SR, please use manual input that can meet the delay time requirement. If you could not input manually, please follow the flow, " Wait for MDIO_CFG[BSY] = 0" before read MDIO_DATA value. Read SGMII1 MDIO Registers === Serdes Test 1 === 0xFFE0EA8FC value: 0x08000000 Dump PCS0 Registers 0xFFE4E1030-0xFFE4E103C: 0x40001408 0x00000000 0x00001340 0x00001340 Select 0x8002 ,devmem 0xFFE4E1034 32 0x8002 Read: 0x00000083 Select 0x8003 ,devmem 0xFFE4E1034 32 0x8003 Read: 0x0000E400 Select 0x8001 ,devmem 0xFFE4E1034 32 0x8001 Serdes0 Status: 0x00000029 Select 0x8001 devmem 0xFFE4E1034 32 0x8001 Serdes0 Status: 0x0000002D Select 0x8001, devmem 0xFFE4E1034 32 0x8001 Serdes0 Status: 0x0000002D The first time, it’s not link, LINK_STAT is 0(0x00000029), and then it’s turn to 1(0x0000002D). Now the PCS link up and the HW loopback checking is completely.
查看全文
Issue description. The CodeWarrior ®  TAP enables target system debugging via a standard debug port (usually JTAG) while connected to a developer's workstation via Ethernet or USB. This the hardware debug tool(JTAG debug tool) to debug the DN MPU. You could find the tool from below link https://www.nxp.com/design/design-center/development-boards-and-designs/CW_TAP To debug the Layerscape MPU, should select CWH-CTP-BASE-HE and CWH-CTP-CTX10-YE In fact, the CWH-CTP-CTX10-YE will adapt the different signal definition, one connector will be insert to the CWH-CTP-BASE-HE, and another one(totally 10 pins) will be used to debug the Layerscape MPU. You could find the definition of the JTAG connector(CWH-CTP-CTX10-YE, 10pins) on the Layerscape board. Pin 10 (SRST)is the signal of this documents to should add workaround.     In the CodeWarrior TAP Probe User Guide, the SRST(SRST_B) is Open-drain. So the voltage of this signal should be decided by the pull-up voltage connect to it. See the schematics part below, pin 10 (JTAG_RST_B) should be 1.8V, but in fact it’s not.   Layer define.png The test signal will be exceed 1.8V to about 2.6V.   issue.png If you connect this pin directly to the Layerscape MPU, it will violate the SPEC of the VIN. Workaround. Workaround for the user would be to use an external circuit (level shifter/limiter) for the affected signal(s). level-shifter/limiter CWTAP <=> probe tip <=> (level-shifter/limiter) <=> target Please refer to FRWYLS1046A-PA,  use the AND gate 74AUP1G11GW similar components which the Overvoltage tolerant inputs to 3.6 V.   issueworkaround.png   Logic Device Customer could also refer to LS1046ARDB CPLD LCMXO1200C-3FTN256C and LX2160ARDB CPLD EPM2210F256C5N, even the CPLD IO Voltage is 1.8V, no issue with 2.6V input on 1.8V IO ports.    
查看全文
LS1043ARDB version updated because we replaced the Nand Flash with different page size one as the old one is obsolete. Version update information FA version Nand flash program by CodeWarrior Nand Flash firmware bring up files Boot Mode setting
查看全文
In the LS1028ARDB, SPI is not enable, some customers need to enable this interface to debug their device and some customer maybe enable this device but the SPI sequence would be some uncertain error which will delay their plan. In this documents, will introduce how to enable the SPI3 on the LS1028ARDB, and use a SPI tools in the LSDK to help customer debug their SPI device in the initial stages of debugging.
查看全文
The CodeWarrior tool – QCVS SerDes tool allows you to configure the SerDes block and provides you a GUI application to validate the SerDes configuration.  QCVS SERDES supports LX2 but except Serdes#1 Lane H, customer can use the guide below for Tx pattern generation. 
查看全文
SECURE BOOT Secure Boot introduction Build secure boot ATF image Generate secure boot CSF headers for Linux tiny itb image Deploy secure boot images on the target board Blow OTPMK fuse in u-boot and through CodeWarrior CCS Write SRK hash keys to the mirror registers through CCS Secure boot Trouble Shooting  Fuse Provisioning Fuse Provisioning Utility Introduction Input File for Fuse Provisioning Tool Build Fuse Provisioning Firmware Image with flex-builder and Deploy the Firmware Image Build and Deploy Fuse Provisioning Image Manually Validate Fuse Provisioning Secure Debug Program DCVR and DRVR fuses to activate secure debug Unlock JTAG debug port after locking it through CCS commands Unlock JTAG debug port after locking it through CW IDE  
查看全文
PPS (Pulses Per Second) signal applies to most network controllers of Layerscape, including DPAA1 platforms. PPS signal is output through 1588 timer pulse out pin. The QorIQ PTP driver configured fixed interval period pulse (FIPER) generator as PPS signal in default. This document describes how to create dts file to customize configuration on the 1588 timer such as selecting other reference clock source, and configuring nominal clock period, FIPERs period, and output clock period to generate the required PPS signal.
查看全文
Compile kernel in the ls-5.15.71-2.2.0_distro In the LLDPUG_RevL5.15.71-2.2.0, it seems when do some reconfiguration in the kernel, rootfs should be repack to finish the change. Here will generate kernel without repack the roofts in the Linux host machine just compile the kernel.
查看全文
The SerDes tool is a part of the QorIQ Configuration and Validation Suite (QCVS) product. This document will illustrate how to use the tools to validate the SerDes on the LS1046ARDB SerDes1 Lane1(Lane C) without Oscilloscope and BERT(Bit Error Ratio Tester). It validate the LS1046ARDB SerDes1 Lane1 with digital loopback, external loopback and external mode.
查看全文
Basic Concept of Secure boot on LS1028A Platform Build secure boot ATF image Generate secure boot CSF headers for Linux tiny itb image Deploy secure boot images on the target board Blow OTPMK fuse in u-boot and through CodeWarrior CCS Write SRK hash keys to the mirror registers through CCS Secure boot Trouble Shooting  
查看全文