LS1043ARDB Ethernet and FMC port mapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB Ethernet and FMC port mapping

LS1043ARDB Ethernet and FMC port mapping

The table below shows the mapping of the Ethernet port names appearing on the front panel of the LS1043ARDB chassis with the port names in U-Boot, tinyDistro, and NXP LSDK userland. 

Ethernet port mapping
Port name on chassisPort name in U-BootPort name in Linux (tinyDistro)Port name in Linux (LSDK
userland)
QSGMII.P0FM1@DTSEC1eth0fm1-mac1
QSGMII.P1FM1@DTSEC2eth1fm1-mac2
QSGMII.P2FM1@DTSEC3eth2fm1-mac5
QSGMII.P3FM1@DTSEC4eth3fm1-mac6
RGMII1FM1@DTSEC5eth4fm1-mac3
RGMII2FM1@DTSEC6eth5fm1-mac4
10G CopperFM1@TGEC1eth6fm1-mac9

Below is a table that shows the mapping between port numbers (from configuration file), character devices, hardware ports
(Rx) and mEMACs for the standard SDK configuration (using RCW protocol 1455).

FMC port mapping
Port name on chassisXML port number (configuration file)Serdes protocolCharacter deviceHardware port
(device tree node)
mEMAC (device tree
node)
QSGMII.P01qsgmiifm0-port-rx0port@88000ethernet@e0000
QSGMII.P12qsgmiifm0-port-rx1port@89000ethernet@e2000
QSGMII.P25qsgmiifm0-port-rx4port@8c000ethernet@e8000
QSGMII.P36qsgmiifm0-port-rx5port@8d000ethernet@ea000
RGMII13rgmiifm0-port-rx2port@8a000ethernet@e4000
RGMII24rgmiifm0-port-rx3port@8b000ethernet@e6000
10G Copper9xgmiifm0-port-rx6port@90000ethernet@f0000
Labels (1)
100% helpful (2/2)
Version history
Last update:
‎05-22-2019 09:59 PM
Updated by: