LS1028 Felix Switch Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028 Felix Switch Configuration

LS1028 Felix Switch Configuration

On successful probing of the DSA Felix switch, each available front panel switch port should have a network device interface attached with the swpX name format. The ip link show command uses the swpX@enoY name format to also indicate the associated master Ethernet interface for the DSA switch port, which corresponds to an internal ENETC interface, usually the eno2 (Port2) for the LS1028A SoC.

LS1028 Interface naming in Linux

Single port mode

Bridge mode

添付
コメント

useful

100%が役に立ったと言っています (4/4)
バージョン履歴
最終更新日:
‎10-14-2020 02:20 AM
更新者: