LS1028 Felix Switch Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028 Felix Switch Configuration

LS1028 Felix Switch Configuration

On successful probing of the DSA Felix switch, each available front panel switch port should have a network device interface attached with the swpX name format. The ip link show command uses the swpX@enoY name format to also indicate the associated master Ethernet interface for the DSA switch port, which corresponds to an internal ENETC interface, usually the eno2 (Port2) for the LS1028A SoC.

LS1028 Interface naming in Linux

Single port mode

Bridge mode

Attachments
Comments

useful

100% helpful (3/3)
Version history
Last update:
‎10-14-2020 02:20 AM
Updated by: