How to use UART2 instead of UART1 on LS1043ARDB/LS1046ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use UART2 instead of UART1 on LS1043ARDB/LS1046ARDB

How to use UART2 instead of UART1 on LS1043ARDB/LS1046ARDB

How to use UART2 instead of UART1 on LS1043ARDB/LS1046ARDB.

 

1. Compile PBL binary from RCW source file

2. Compile U-Boot binary

3. Compile TF-A binaries (bl2_.pbl and fip.bin)

4. Program TF-A binaries on specific boot mode

 

 

1-COMPILE PBL BINARY FROM RCW SOURCE FILE

 

You have to create a new directory to compile the binaries that you need to create a

TF-A binary

You need to compile the rcw_<boot_mode>.bin binary to build the

bl2_<boot_mode>.pbl binary.

 

Clone the rcw repository and compile the PBL binary.

 

1. $ git clone https://github.com/nxp-qoriq/rcw

2. $ cd rcw

3. $ cd ls1043ardb

4. $ make

 

Inside the directory called “RR_FQPP_1455” you can see some binaries with

the next nomenclature:

rcw_<freq>.bin

Where “freq” is the frequency in MHz of the processor, the values of the frequency

are 1200MHz, 1400MHz, 1500MHz, and 1600MHz

 

2-COMPILE U-BOOT BINARY

You need to compile the u-boot.bin binary to build the fip.bin binary.

Clone the U-boot repository and compile the U-Boot binary for TF-A

 

1. $ git clone https://github.com/nxp-qoriq/u-boot

2. $ cd u-boot

3. $ git checkout -b LSDK-21.08 LSDK-21.08

4. $ export ARCH=arm64

5. $ export CROSS_COMPILE=aarch64-linux-gnu-

6. $ make distclean

7. $ nano configs/ls1043ardb_tfa_defconfig

7.1 change the bootargs "console=ttyS0,115200" for "console=ttyS1,115200"

7.2 add "CONFIG_CONS_INDEX=2

7. $ make ls1043ardb_tfa_defconfig

8. $ make

 

3 Compile TF-A binaries (bl2_.pbl and fip.bin)

1. $ git clone https://github.com/nxp-qoriq/atf

2. $ cd atf

3. $ git checkout -b LSDK-21.08 LSDK-21.08

4. $ export ARCH=arm64

5. $ export CROSS_COMPILE=aarch64-linux-gnu-

6. $ nano plat/nxp/common/include/default/ch_3_2/soc_default_base_addr.h

6.1 Change the line "#define NXP_UART_ADDR 0x021C0000" for "#define NXP_UART_ADDR 0x021D0000"

6.2 Change the line "#define NXP_UART1_ADDR 0x021D0000" for "#define NXP_UART_ADDR 0x021C0000"

 
7. $ nano plat/nxp/common/include/default/ch_2/soc_default_base_addr.h

7.1 Change the line "#define NXP_UART_ADDR 0x021C0500" for "#define NXP_UART_ADDR 0x021C0600"

7.2 Change the line "#define NXP_UART1_ADDR 0x021C0600" for "#define NXP_UART_ADDR 0x021C0500"

 

The compiled BL2 binaries, bl2.bin and bl2_<boot mode>.pbl are available at

atf/build/ls1043ardb/release/.

NOTE: For any update in the BL2 source code or RCW binary, the bl2_<boot

mode>.pbl binary needs to be recompiled

 

3.1 HOW TO COMPILE BL2 BINARY

To compile the BL2 binary without OPTEE:

make PLAT=<platform> bl2 BOOT_MODE=<boot_mode> pbl

RCW=<path_to_rcw_binary>/<rcw_binary_for_specific_boot_mode>

 

To LS1043ARDB for SD boot:

make PLAT=ls1043ardb bl2 BOOT_MODE=sd pbl

RCW=<path_to_rcw_binary>/<rcw_freq.bin>

 

To LS1043ARDB for NOR boot:

make PLAT=ls1043ardb bl2 BOOT_MODE=nor pbl

RCW=<path_to_rcw_binary>/<rcw_freq.bin>

 

To LS1043ARDB for NAND boot:

make PLAT=ls1043ardb bl2 BOOT_MODE=nand pbl

RCW=<path_to_rcw_binary>/<rcw_freq.bin>

 

3.2 HOW TO COMPILE FIP BINARY

 

To compile the FIP binary without OPTEE and trusted board boot:

$make PLAT=<platform> fip BL33=<path_to_u-boot_binary>/u-boot.bin

 

For LS1043ARDB:

$make PLAT=ls1043ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin

 

The compiled BL31 and FIP binaries ( bl31.bin, fip.bin ) are available at

atf/build/ls1043ardb/release/. For any update in the BL31, BL32, or BL33 binaries,

the fip.bin binary needs to be recompiled.

 

4 Program TF-A binaries on specific boot mode

For that step you can use a tftp server, but it is easier with a USB formatted on

FAT32.

 

You have to put the files “ bl2_<boot_mode>.pbl” and “fip.bin” in the usb and follow

the steps to your boot mode.

 

4.1 Program TF-A binaries on IFC NOR flash

For LS1043A, the steps to program TF-A binaries on IFC NOR flash are as follows:

 

1. Boot the board from the default bank.

2. Under U-boot prompt:

=> usb start

3. Flash bl2_nor.pbl:

=> fatload usb 0:1 $load_addr bl2_nor.pbl

 

a. Alternate bank:

=> protect off 64000000 +$filesize && erase 64000000 +$filesize &&

cp.b $load_addr 64000000 $filesize

 

b. Current bank:

=> protect off 60000000 +$filesize && erase 60000000 +$filesize &&

cp.b $load_addr 60000000 $filesize

 

 

4. Flash fip.bin:

=> fatload usb 0:1 $load_addr fip.bin

 

a. Alternate bank:

=> protect off 64100000 +$filesize && erase 64100000 +$filesize &&

cp.b $load_addr 64100000 $filesize

 

b. Current bank:

=> protect off 60100000 +$filesize && erase 60100000 +$filesize &&

cp.b $load_addr 60100000 $filesize

 

5. Reset your board:

 

a. Alternate bank:

cpld reset altbank

 

b. Current bank:

cpld reset

 

4.2 Program TF-A binaries on NAND flash

 

1. Boot the board from the default bank.

 

2. Under U-boot prompt:

=> usb start

 

3. Flash bl2_nand.pbl to NAND flash:

 

=> fatload usb 0:1 $load_addr bl2_nand.pbl

=> nand erase 0x0 $filesize;nand write $load_addr 0x0 $filesize;

 

4. Flash fip_uboot.bin to NAND flash:

 

=> fatload usb 0:1 $load_addr fip.bin

=> nand erase 0x100000 $filesize;nand write $load_addr 0x100000 $filesize;

 

5. Reset your board:

=> cpld reset nand

 

4.3 Program TF-A binaries on SD card

 

To program TF-A binaries on an SD card, follow these steps:

 

1. Boot the board from the default bank.

 

2. Under U-boot prompt:

=> usb start

 

3. Flash bl2_sd.pbl to SD card:

=> fatload usb 0:1 $load_addr bl2_sd.pbl

=> mmc write $ load_addr 8 A1

 

4. Flash fip.bin to SD card:

=> fatload usb 0:1 $load_addr bl2_sd.pbl

=> mmc write $load_addr 800 A1

 

5. Reset your board:

=> cpld reset sd

Now the console should be out from UART2 port of the board.

Chavira_0-1698856099543.png

 

ラベル(1)
100%が役に立ったと言っています (2/2)
バージョン履歴
最終更新日:
‎11-22-2023 09:05 AM
更新者: