Mouse Device example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mouse Device example

Mouse Device example

Description

This example implements a HID class device with mouse report descriptors. Mouse movement reports are sent to the host by the device when buttons or the joystick is pressed on the development board.

 

On the Embedded Artists LPCXpresso Rev A or B Baseboard this example will move the host PC's mouse cursor when the joystick is operated. Pressing the joystick down will create a mouse left click.


Compiler build configurations

The software that makes up this example is designed to run on many different development boards. Therefore the compiler must be configured to build an image that is targeted to the development board you are using. This section explains how to set these build configurations for each of the supported compilers.

 

LPCXpresso IDE

Configure projects

  right click on the BSP project in the project explorer window
  click Build Configurations->Set Active->(see configuration in table below)
  repeat these steps with the CDL, nxpUSBlib, and Example_MouseDevice

Configure MCU

  right click on the Example_MouseDevice project in the project explorer window
  click Properties->C/C++ Build->MCU settings->(see configuration in table below)

Configure the indexer

   click Window->Preferences->C/C++->Indexer->Use active build configuration

BSP

CDL

nxpUSBlib

Example_MouseDevice

MCU

LPC1850  / Hitex

LPC18xx_HITEX

LPC18xx

LPC18xx_Device

LPC18xx

LPC1850

LPC4330  / Xplorer

LPC4330_Xplorer

LPC18xx

LPC18xx_Device

LPC18xx

LPC4330

LPC4350  / Element14

LPC1435_ELEMENT14

LPC18xx

LPC18xx_Device

LPC18xx

LPC4350

LPC11U14 / LPCXpresso

LPC11Uxx_LPCXpressoRevB

LPC11Uxx

LPC11Uxx_Device

LPC11Uxx

LPC11U14

LPC11U14 / MCB1000

LPC11u14_MCB1000

LPC11Uxx

LPC11Uxx_Device

LPC11Uxx

LPC11U14

LPC1768  / MCB1700

LPC1768_MCB1700

LPC17xx

LPC17xx_Device

LPC17xx

LPC1768

LPC1768  / LPCXpresso

LPC17xx_LPCXpressoRevB

LPC17xx

LPC17xx_Device

LPC17xx

LPC1768


NOTE:
The LPC18xx CDL is used with boards that hold LPC43xx parts. This is done because the LPC43xx CDL is currently experimental. The LPC18xx USB library is used because both parts share the same controller.

 

Keil uVision 4 IDE

Configure a Batch Build

 

  click on Project->Batch Build...
  expand the BSP project to display a list of project targets
  select the project target by checking the appropriate checkbox (see target list in table below)
  repeat these steps with the CDL, nxpUSBlib_Device, and Example_MouseDevice

BSP

CDL

nxpUSBlib_Device

Example_MouseDevice

LPC1850  / Hitex

HITEX1800

LPC18xx

LPC18xx_Device

HITEX1800

LPC1768  / MCB1700

MCB1700

LPC17xx

LPC17xx_Device

MCB1700

LPC11U14 / MCB1000

MCB1000

LPC11Uxx

LPC11Uxx_Device

MCB1000

 

Board connections and configurations

 

LPC18xx_HITEX (LPC1850 Hitex Evaluation Board)  older A2 design

schematic ./BSP/schematics/HITEX_SCM_LPC1850EVA-A2-2.pdf

 

Connect the JTAG to the 20 pin receptacle marked X4 JTAG
Connect the type-B end of a USB cable to the receptacle marked X2. Plug the type-A end of this cable into a PC

LPC18xx_HITEX (LPC1850 Hitex Evaluation Board)  newer A4 design

schematic ./BSP/schematics/HITEX_Final_LPC1850EVA-A3.pdf

 

LPC4330_Xplorer (NGX Xplorer Evaluation Board with LPC4330)

Connect the JTAG to the 10 pin receptacle marked J2
Connect the micro-b end of a USB cable to the receptacle marked USB0. Plug the type-A end of this cable into a PC

 

LPC1435_ELEMENT14 (Element 14 gaming board with LPC4350)

Connect the JTAG to the 10 pin receptacle marked J6
Connect one end of a type-A to type-A USB cable to the receptacle marked USB0. Plug the other end of this cable into a PC

 

LPC11u14_MCB1000 (Keil MCB1000 development board)

schematic: ./BSP/schematics/mcb1000-schematics.pdf

 

Jumpers:
  J4 = 2-3      (UCON - PIO0_6 pulls D+ high)
  J2 = 1-2          (VDD  - core power)
  J5 not installed  (ISP  - ISP via COMM)
  J6 not installed  (RST  - ISP via COMM)
Connect the JTAG debugger to the 10 pin Cortex Debug connector labeled J3
Connect the type-B end of a USB cable to the type-B recepticle and the type-A end of the cable to the USB receptacle on a PC
Once the USB cable is connected to the board the following LEDs should be illuminated:
    Power
    All 8 LEDs in PIO2

 

LPC1768_MCB1700 (Keil MCB1700 development board)

schematic: ./BSP/schematics/mcb1700-schematics.pdf

 

Jumpers:
  E/U    = 1-2  (Ethernet/USB)
  UMODE  = 1-2  (USB Device Mode)
  D-     = Device
  D+     = Device
  VBUS   = 1-2
  VDDIO  = 1-2
  VDDREG = 1-2
 
Connect the JTAG debugger to the 20 pin JTAG or 10 pin Cortex Debug connector.
Connect the type-B end of a USB cable to the type-B recepticle labeled 'Device' and the type-A end of the cable to the USB receptacle on a PC. Once the USB cable is connected to the board the following LEDs should be illuminated:
    Power
    100MHz
    USC (LED indicates a USB soft connect from P2.9)
  

LPC11Uxx_LPCXpressoRevB (LPCXpresso LPC11Uxx on the LPCXpresso Rev B base board)

schematic: ./BSP/schematics/lpcxpresso.lpc11u14.schematic.pdf

 

Running this example on the LPCXpresso LPC11U14 can be done one of two ways:

 

1. LPCXpresso LPC11U14 stand-alone
      Connect the type-B end of a USB cable to the mini receptacle on the LPCXpresso board labeled J8 and the type-A end to the USB receptacle on a PC

 

2. LPCXpresso LPC11U14 plugged into the LPCXpresso base board Rev B
      Plug the LPCXpresso LPC11U14 board into the connector labeled J4 on a LPCXpresso base board Rev B
      Configure the base board according to the user's guide from Embedded Artists
      Connect the mini type-B end of a USB cable to the receptacle on the base board labeled X1 and the type-A end to the USB receptacle on a PC
      Once the USB cable is connected to the board the following LEDs should be illuminated:
          LED25  (vbus)
         LED26  (3.3v rail)
       
For both configurations the JTAG debugger is connected to the mini USB receptacle labeled J3 on the LPCXpresso LPC11U14 board

 

LPC17xx_LPCXpressoRevB (LPCXpresso LPC17xx on the LPCXpresso Rev B base board)

schematic: ./BSP/schematics/LPCXpressoLPC1769revB.pdf

 

Running this example on the LPCXpresso LPC1769 can be done one of two ways:

 

1. LPCXpresso LPC1769 stand-alone. Solder a type-B USB receptacle onto the board and wire it up. See included schematics for details. Connect the type-B end of a USB cable to the receptacle on the LPCXpresso board and the type-A end to the USB receptacle on a PC

 

2. LPCXpresso LPC1769 plugged into the LPCXpresso base board Rev B. Plug the LPCXpresso LPC1769 board into the connector labeled J4 on a LPCXpresso base board Rev B. Configure the base board according to the users guide from Embedded Artists. Connect the mini type-B end of a USB cable to the receptacle on the base board labeled X1 and the type-A end to the USB receptacle on a PC.
  
Once the USB cable is connected to the board the following LEDs should be illuminated:
      LED25  (vbus)
      LED26  (3.3v rail)
       
For both configurations the JTAG debugger is connected to the mini USB receptacle labeled J3 on the LPCXpresso LPC1769 board.

 

PC configuration

Use a PC running Windows XP, Vista or 7 Connect the type-A end of the USB cable that is connected to the board into one of the USB receptacles on the PC

Build and debug the example


LPCXpresso IDE

In the project explorer window of the IDE right click on the Example_MouseDevice project and select Debug As->C/C++ MCU Application
In the main window of the IDE click Run->Resume to start running the application

 

Keil uVision 4 IDE

In the Batch Build window, select the project targets as described in Compiler Build Configurations and then click Build
In the main window of the IDE click Debug->Start/Stop Debug Session click Debug->Run

 

How this example runs and what to look for

When the example is run and the board is connected to a PC with a USB cable it will enumerate on the PC as a HID Mouse device. You should see the device appear in the "Device Manager" under "Mice". If you right click on HID  Device->Properties a window will appear called "HID Mouse Device Properties". If you select the "Details" tab you will see a "Properties" drop down, click on it and select "Hardware Ids". You should see the below entries for Vendor Id and Product Id.

 

HID\VID_1FC9&PID_2041&REV_0001
HID\VID_1FC9&PID_2041

 

This information should match the data in the "Device Descriptor Structure" in the "Descriptors.c" file in the Example_MouseDevice project directory.

 

Press the joystick to move the mouse cursor on the PC desktop and push the buttons to cause mouse buttons to click.

評価なし
バージョン履歴
最終更新日:
‎04-25-2016 02:23 PM
更新者: