which CMSIS library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

which CMSIS library

854件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nw002 on Wed Feb 01 05:53:23 MST 2012
Hi All,

I am a newbie to LPCXpresso so please bear with me : I have tried searching the forums and code_red but no joy.

My question - when you import a CMSIS project into LPCXpresso, you get a choice of different libraries (ZIP files) to select. For my target device (LPC1114-301), there seems to be 4 choices that are relevant :

CMSISv1p30_LPC11xx.zip
CMSISv2p00_LPC11xx.zip
LPCXpresso1114_cmsis2.zip
NXP_LPCXpresso1114-301_2011-01-27.zip

What are the differences between these libraries?

How do I know which one I should use?

Can someone point me at the relevant documentation?

thanks
Nick
0 件の賞賛
返信
1 返信

812件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Feb 01 06:07:10 MST 2012
See http://support.code-red-tech.com/CodeRedWiki/SuppliedExamples

Regards,
CodeRedSupport
0 件の賞賛
返信