what to do with old LPC17xx.h files when integrating sofware in new project?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what to do with old LPC17xx.h files when integrating sofware in new project?

566 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xjx on Mon Dec 14 15:10:37 MST 2015
Hello,

I have LPCopen project running, and would like to add preexistent code to manage the EEPROM onboard the LPC1769 stick.

However, the new code makes reference to LPC17xx.h, which is not present in LPCOpen projects. On the other hand, LPCOpen projects looks like have replaced LPC17xx.h library with something else.

any comments on how to proceed?

regards
xJx
0 项奖励
回复
2 回复数

551 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xjx on Fri Dec 18 06:45:50 MST 2015

Quote: R2D2

No idea which hardware you are talking about  :O





No idea? :bigsmile:  it is soldered close to the uC in the LPCxpresso, it is the microchip 24xx64.



Quote:
  You'll find several threads about LPC17xx and I2C EEPROMs...



I know!!! however I am looking for a solved case. As the board comes with 24xx64 EEPROM soldered in the same board the uC is, I am sure somebody else has done this job,


0 项奖励
回复

551 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Dec 14 15:20:38 MST 2015

Quote: xjx
...the EEPROM onboard the LPC1769 stick...



:quest:


Quote: xjx
any comments on how to proceed?



No idea which hardware you are talking about  :O

LPCOpen is including an I2C Sample, so if your EEPROM is an I2C EEPROM this code is working...

You'll find several threads about LPC17xx and I2C EEPROMs...

0 项奖励
回复