variable not refeshed or updated sync (without build)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

variable not refeshed or updated sync (without build)

739 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by riscy00 on Sun Jan 26 04:28:08 MST 2014
When I add new variable name within enum, typedef struct or just variable and so on (I call it symbol). I inserted variable/symbol in elsewhere but does not change to blue nor recognised, nor include symbol in the list (when hover on above symbol).

Most complier has automatic refresh or updated when new symbol is added. This IDE does not. To get it updated I had to rebuild which is not ideal way to do this because I have not finish coding and would generate complier error (and stop processing code/update symbol table?).

I looked into "update", "refresh" in help but did not gave any correct answer that make sense.

below is an example

ALPS_NAV_OP.
ALPS_NAV_OP.RotaryState=ALPS_Neutral;

I had to manually insert RotaryState and ALPS_Neutral symbol after change within enum and typedef struct in header filename or other code filename because the symbol table is not updated. It is annoying to type manually.

R. 

0 Kudos
Reply
1 Reply

731 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Jan 26 05:11:17 MST 2014
Try saving the file - that should cause the indexer to refresh. If not, right-click on the project and select Index->Rebuild.
0 Kudos
Reply