usb host mode for LPC1769

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb host mode for LPC1769

652 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mayur.p.85 on Thu Jun 06 11:29:21 MST 2013
Hi All

I would like to use USB controller of LPC1769 in host mode. I got the confusion that if I use the 4 USB wires of Mini - B USB cable to connect to the LPCXpresso 1769 board than whether that would be ok or not?

Regards,
Mayur
0 Kudos
Reply
1 Reply

602 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Jun 06 11:48:55 MST 2013

Quote: mayur.p.85
I got the confusion that if I use the 4 USB wires of Mini - B USB cable to connect to the LPCXpresso 1769 board than whether that would be ok or not



It's OK to use an USB2.0 cable :)
0 Kudos
Reply