usb host mode for LPC1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb host mode for LPC1769

651件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mayur.p.85 on Thu Jun 06 11:29:21 MST 2013
Hi All

I would like to use USB controller of LPC1769 in host mode. I got the confusion that if I use the 4 USB wires of Mini - B USB cable to connect to the LPCXpresso 1769 board than whether that would be ok or not?

Regards,
Mayur
0 件の賞賛
返信
1 返信

601件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Jun 06 11:48:55 MST 2013

Quote: mayur.p.85
I got the confusion that if I use the 4 USB wires of Mini - B USB cable to connect to the LPCXpresso 1769 board than whether that would be ok or not



It's OK to use an USB2.0 cable :)
0 件の賞賛
返信