uTasker compiled in LPCXpresso_7.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uTasker compiled in LPCXpresso_7.3

849 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kiryat8 on Tue Aug 19 03:58:59 MST 2014
Shalom!
Is it possible to compile and debug an uTasker project in the  LPCXpresso_7.3 IDE?
The uTasker project has several features that I would like to use in my project.

The uTasker project will build from a GCC make file so may able to work
with Code Red (I believe that Code Red is an Eclipse based environment
using GCC).


Has anyone tried?

Thanks
0 Kudos
Reply
2 Replies

842 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Wed Aug 20 11:54:09 MST 2014
The web sites says there is a LPC17xx port.
But it is not free for commercial use.
there are other free options as well.
http://en.wikipedia.org/wiki/List_of_ARM_Cortex-M_development_tools
0 Kudos
Reply

842 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 20 02:24:45 MST 2014
Yes LPCXpresso uses GCC as its compiler toolchain. Thus if the code base was written for GCC, then you should be able to get it building. However we have no direct experience of uTasker.

(FYI - Code Red Technologies was the company that originally produced LPCXpresso, but is now part of NXP)

Regards,
LPCXpresso Support
0 Kudos
Reply