uLINK Pro Debug and Trace Unit with LPCXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uLINK Pro Debug and Trace Unit with LPCXpresso

2,879件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Wed Jun 24 06:31:24 MST 2015
Can we use uLINK Pro with LPCXpresso(version 7.8.0-426)?
0 件の賞賛
返信
10 返答(返信)

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 29 00:42:33 MST 2015
Please re-read the LPCXpresso V1 boards page I pointed you at. To quote:


Quote:
Cutting the tracks between the LPC-Link and the target will change the LPC-Link into a standalone JTAG/SWD debug probe



There is even a video on that page showing this!

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Sun Jun 28 21:40:20 MST 2015
There is no LPCXpresso board available with LPC3250 target.
Is it possible to get LPC Link as a stand-alone debug probe?
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jun 26 08:35:27 MST 2015
If you read the FAQ previously referenced and follow the links it contains, you will see that LPC-Link is the built in debug probe provided by the original LPCXpresso boards:

http://www.lpcware.com/LPCXpressoV1Boards

These are very, very widely available from lots of distributors.

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Thu Jun 25 23:05:42 MST 2015
We are not in a position to change the part. Also we are not interested to use Red Probe+.
Who is the authorized distributor for LPC-Link in India? Is this product still under support?
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jun 25 09:11:02 MST 2015
As per the FAQ I previously point you at, you can use the original LPC-Link (or a Red Probe+ if you can acquire one).

Note that generally, I wouldn't recommend using the old ARM9 based parts for new designs. You would probably do better looking at something like an LPC43xx.

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Thu Jun 25 04:54:27 MST 2015
I need to connect to LPC3250 using JTAG interface from LPCExpresso. Which debug probe can be used for this?
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Jun 25 00:55:11 MST 2015

Quote: jubiamathew
Does ARM 9 processors(LPC3250) support CMSIS-DAP. Or it is supported onmly by ARM Cortex processors?


This may help
http://www.keil.com/support/man/docs/dapdebug/dapdebug_introduction.htm

Arm9 and Arm 7 do not have Coresight...
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jun 24 23:40:04 MST 2015
Suggest you read...

http://www.lpcware.com/content/faq/lpcxpresso/supported-debug-probes-mcus

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jubiamathew on Wed Jun 24 23:19:33 MST 2015
Does ARM 9 processors(LPC3250) support CMSIS-DAP. Or it is supported onmly by ARM Cortex processors?
0 件の賞賛
返信

2,692件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jun 24 06:47:18 MST 2015
For Debug, LPCXpresso supports CMSIS-DAP. So, if your uLink is loaded with the latest CMSIS-DAP firmware, then it will be supported.

LPCXpresso supports SWO Trace with the LPC-Link2 version of CMSIS-DAP, but not with any others. This is because CMSIS-DAP does not define a SWO Trace interface, so this is an NXP-only extension.
0 件の賞賛
返信