timer in LPC1769

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

timer in LPC1769

909 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by koceila882 on Tue Apr 17 11:03:47 MST 2012
hello friends
I want to use a timer to count a time between an ultrasound transceiver and ultrasound receiver?
How can I use timer in this application ?
thank you
0 Kudos
Reply
1 Reply

876 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue Apr 17 23:45:35 MST 2012
Hi,

You are probably interested in the capture mode. Basically this mode lets you take a snapshot of the timer value on a external event (pin change).

You will need to have a digital input signal, signalling if there is, or if there is no ultrasound received. Let's assume a high signal if there is an ultrasound, and a low signal if there is none.

First you would inititalize the timer in capture mode to take the snapshot of the timer value on a rising edge of your "ultrasound present" signal and generate an interrupt on this event. More information on this can be found in the user manual, chapter 21. Then you can reset the timer value to 0, start the timer and enable the ultrasound transceiver. After this you will only have to wait for the capture interrupt and read the capture value.

Regards,
0 Kudos
Reply