simple Ethernet example [LPC1769]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

simple Ethernet example [LPC1769]

4,987件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Mon Nov 10 14:57:34 MST 2014
Hello everyone!

I'm trying to send any data from my LPCXPRESSO LPC1769 to PC via Ethernet. I tried to use ethernet example, but it doesn't work for me and I don't know why. On UART i receive bunch of random signs:

•ZŁĚĚ úwµ`ŃóŢÄ:úwµç曓8 Ńĺ¬hSSJ/¬)ŚâekúO)Z±Śýwµ`ŃóŢć1ú!k)ŃóŢÄ8šw͡«ˇ«Ś§‡­9žú+ƵýŐkˇú)öŁj!•)8 [ĚŐ°Âć1“Ł
Rő+:řŐkôŁ•Lá!•”)ĚĚ Š7W.r)ˆwµ!v)öŁ#ř!k)ŃóËÄŚýek%úĆZ±Q[qX9ÜŐ°/‰ńá–ęwµçŁ•˛H+ď™§°Ç#Đ”2Üţ!k!r)ˆ¤{FF}ekúO)Z±ŚýŐkôĘĺLCŕ!•)Ěęwµ!ѢŢć;úŐ°ďG<×çŠg©)ŃóŢÄ: ďŃ/3Ĺó ó!•ZŁĚĚŔ{FF}Őkˇr)öŁkůwµ`ŃóŢÄ:úwµçŁ•˛9·rCIb])‹Ĺ_Büeď•/°·#ČńŐ°) >jO)ĚŮŠËÚZ)§°ÇŁ{FF}!k!sâĐ!#YS

°·#Č,2­řpYÖ­9·2


On what IP should i wait for data? I'm using Hercules 3.2.8 to listen to UART TCP and stuff.
Can anyone lead me through simple ethernet example?
0 件の賞賛
返信
10 返答(返信)

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Tue Nov 11 06:46:28 MST 2014
damn my fault. I checked my terminal and i didn't change baudrate. With 115200 baudrate i receive from UART something like that:
Packet received: -Dest MAC: 33:33:00:01:00:03--Source MAC: 1c:75:08:cc:9c:d1--Packet len: 86-Type: 86dd
Packet received: -Dest MAC: 01:00:5e:00:00:fc--Source MAC: 1c:75:08:cc:9c:d1--Packet len: 66-Type: 0800
Packet received: -Dest MAC: ff:ff:ff:ff:ff:ff--Source MAC: 1c:75:08:cc:9c:d1--Packet len: 92-Type: 0800
Packet received: -Dest MAC: ff:ff:ff:ff:ff:ff--Source MAC: 1c:75:08:cc:9c:d1--Packet len: 92-Type: 0800
Packet received: -Dest MAC: ff:ff:ff:ff:ff:ff--Source MAC: 1c:75:08:cc:9c:d1--Packet len: 92-Type: 0800

It's still connected to UART3
Now my question is:
How i can send for example integer via Ethernet, and how i can check and where if it is send? My main intention is to collect data from sensors and send it via Ethernet to PC.
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Nov 11 06:37:44 MST 2014

Quote: Zahoq
so if i understand it right I have to connect any UART to pc port and monitor the port.



Nooooooooooooooooooooooooooooooooooooooooo  :O

Your board library is selecting this UART  :)

If you didn't change board.h your UART is UART[color=#f00]1[/color]....
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Tue Nov 11 06:28:38 MST 2014
i don't setup anything, i'm just running periph_ethernet example which is:
/*
 * @briefSimple ethernet example
 *
 * @note
 * Copyright(C) NXP Semiconductors, 2014
 * All rights reserved.
 *
 * @par
 * Software that is described herein is for illustrative purposes only
 * which provides customers with programming information regarding the
 * LPC products.  This software is supplied "AS IS" without any warranties of
 * any kind, and NXP Semiconductors and its licensor disclaim any and
 * all warranties, express or implied, including all implied warranties of
 * merchantability, fitness for a particular purpose and non-infringement of
 * intellectual property rights.  NXP Semiconductors assumes no responsibility
 * or liability for the use of the software, conveys no license or rights under any
 * patent, copyright, mask work right, or any other intellectual property rights in
 * or to any products. NXP Semiconductors reserves the right to make changes
 * in the software without notification. NXP Semiconductors also makes no
 * representation or warranty that such application will be suitable for the
 * specified use without further testing or modification.
 *
 * @par
 * Permission to use, copy, modify, and distribute this software and its
 * documentation is hereby granted, under NXP Semiconductors' and its
 * licensor's relevant copyrights in the software, without fee, provided that it
 * is used in conjunction with NXP Semiconductors microcontrollers.  This
 * copyright, permission, and disclaimer notice must appear in all copies of
 * this code.
 */

#include "board.h"
#include <stdio.h>
#include <string.h>

/*****************************************************************************
 * Private types/enumerations/variables
 ****************************************************************************/

#define ENET_NUM_TX_DESC 4
#define ENET_NUM_RX_DESC 4

#if defined(CHIP_LPC175X_6X)
#define ENET_RX_DESC_BASE        (0x2007C000)
#else
/* The Ethernet Block can only access Peripheral SRAM and External Memory. In this example,
   Peripheral SRAM is selected for storing descriptors, status arrays and send/receive buffers.*/
#define ENET_RX_DESC_BASE        (0x20000000UL)
#endif
#define ENET_RX_STAT_BASE        (ENET_RX_DESC_BASE + ENET_NUM_RX_DESC * sizeof(ENET_RXDESC_T))
#define ENET_TX_DESC_BASE        (ENET_RX_STAT_BASE + ENET_NUM_RX_DESC * sizeof(ENET_RXSTAT_T))
#define ENET_TX_STAT_BASE        (ENET_TX_DESC_BASE + ENET_NUM_TX_DESC * sizeof(ENET_TXDESC_T))
#define ENET_RX_BUF_BASE         (ENET_TX_STAT_BASE + ENET_NUM_TX_DESC * sizeof(ENET_TXSTAT_T))
#define ENET_TX_BUF_BASE         (ENET_RX_BUF_BASE  + ENET_NUM_RX_DESC * ENET_ETH_MAX_FLEN)
#define ENET_RX_BUF(i)           (ENET_RX_BUF_BASE + ENET_ETH_MAX_FLEN * i)
#define ENET_TX_BUF(i)           (ENET_TX_BUF_BASE + ENET_ETH_MAX_FLEN * i)

STATIC ENET_RXDESC_T *pRXDescs = (ENET_RXDESC_T *) ENET_RX_DESC_BASE;
STATIC ENET_RXSTAT_T *pRXStats = (ENET_RXSTAT_T *) ENET_RX_STAT_BASE;
STATIC ENET_TXDESC_T *pTXDescs = (ENET_TXDESC_T *) ENET_TX_DESC_BASE;
STATIC ENET_TXSTAT_T *pTXStats = (ENET_TXSTAT_T *) ENET_TX_STAT_BASE;

/* Transmit/receive buffers and indices */
STATIC int32_t rxConsumeIdx;
STATIC int32_t txProduceIdx;

/*****************************************************************************
 * Public types/enumerations/variables
 ****************************************************************************/

/*****************************************************************************
 * Private functions
 ****************************************************************************/

/* Local delay function used by the ENET or PHY drivers . This can be
   replaced with something more accurate if needed. */
STATIC void localMsDelay(uint32_t ms)
{
ms = ms * 40000;
while (ms > 0) {
ms--;
}
}

/* Initialize MAC descriptors for simple packet receive/transmit */
STATIC void InitDescriptors(void)
{
int i;

/* Setup the descriptor list to a default state */
memset(pTXDescs, 0, ENET_NUM_TX_DESC * sizeof(ENET_TXDESC_T));
memset(pTXStats, 0, ENET_NUM_TX_DESC * sizeof(ENET_TXSTAT_T));
memset(pRXDescs, 0, ENET_NUM_RX_DESC * sizeof(ENET_RXDESC_T));
memset(pRXStats, 0, ENET_NUM_RX_DESC * sizeof(ENET_RXSTAT_T));

rxConsumeIdx = 0;
    rxConsumeIdx = 0;

/* Build linked list, CPU is owner of descriptors */
for (i = 0; i < ENET_NUM_RX_DESC; i++) {
pRXDescs.Packet = (uint32_t) ENET_RX_BUF(i);
pRXDescs.Control = ENET_RCTRL_SIZE(ENET_ETH_MAX_FLEN);
pRXStats.StatusInfo = 0;
pRXStats.StatusHashCRC = 0;
}
for (i = 0; i < ENET_NUM_TX_DESC; i++) {
pTXDescs.Packet = (uint32_t) ENET_TX_BUF(i);
pTXDescs.Control = 0;
pTXStats.StatusInfo = 0;
}

/* Setup list pointers in Ethernet controller */
Chip_ENET_InitTxDescriptors(LPC_ETHERNET, pTXDescs, pTXStats, ENET_NUM_TX_DESC);
Chip_ENET_InitRxDescriptors(LPC_ETHERNET, pRXDescs, pRXStats, ENET_NUM_RX_DESC);
}

/* Get the pointer to the Rx buffer storing new received frame */
STATIC void *ENET_RXGet(int32_t *bytes)
{
uint16_t produceIdx;
void *buffer;

produceIdx = Chip_ENET_GetRXProduceIndex(LPC_ETHERNET);
/* This doesn't check status of the received packet */
if (Chip_ENET_GetBufferStatus(LPC_ETHERNET, produceIdx, rxConsumeIdx, ENET_NUM_RX_DESC) != ENET_BUFF_EMPTY) {
/* CPU owns descriptor, so a packet was received */
buffer = (void *) pRXDescs[rxConsumeIdx].Packet;
*bytes = (int32_t) (ENET_RINFO_SIZE(pRXStats[rxConsumeIdx].StatusInfo) - 4);/* Remove CRC */
}
else {
/* Nothing received */
*bytes = 0;
buffer = NULL;
}

return buffer;
}

/* Release Rx Buffer */
STATIC void ENET_RXBuffClaim(void)
{
rxConsumeIdx = Chip_ENET_IncRXConsumeIndex(LPC_ETHERNET);
}

/* Get Tx Buffer for the next transmission */
STATIC void *ENET_TXBuffGet(void)
{
uint16_t consumeIdx = Chip_ENET_GetTXConsumeIndex(LPC_ETHERNET);

if (Chip_ENET_GetBufferStatus(LPC_ETHERNET, txProduceIdx, consumeIdx, ENET_NUM_TX_DESC) != ENET_BUFF_FULL) {
return (void *) pTXDescs[txProduceIdx].Packet;
}
return NULL;
}

/* Queue a new frame for transmission */
STATIC void ENET_TXQueue(int32_t bytes)
{
if (bytes > 0) {
pTXDescs[txProduceIdx].Control = ENET_TCTRL_SIZE(bytes) | ENET_TCTRL_LAST;
txProduceIdx = Chip_ENET_IncTXProduceIndex(LPC_ETHERNET);
}
}

/* Check if tranmission finished */
STATIC bool ENET_IsTXFinish(void)
{
uint16_t consumeIdx = Chip_ENET_GetTXConsumeIndex(LPC_ETHERNET);

if (Chip_ENET_GetBufferStatus(LPC_ETHERNET, txProduceIdx, consumeIdx, ENET_NUM_TX_DESC) == ENET_BUFF_EMPTY) {
return true;
}
return false;
}

/*****************************************************************************
 * Public functions
 ****************************************************************************/

/**
 * @briefHandle interrupt from ethernet
 * @returnNothing
 */
void ETH_IRQHandler(void)
{
/* This demo is entirely polled, so the IRQ isn't really needed */
}

/**
 * @briefmain routine for ENET example
 * @returnNothing (function should not exit)
 */
int main(void)
{
uint8_t macaddr[6], *workbuff;
uint32_t physts = 0;
int32_t rxBytes, i;
bool ethpkttgl = true;
volatile int k = 1;

SystemCoreClockUpdate();
Board_Init();

/* LED0 is used for the link status, on = PHY cable detected */
/* Initial LED state is off to show an unconnected cable state */
Board_LED_Set(0, false);

/* Setup ethernet and PHY */
#if defined(USE_RMII)
Chip_ENET_Init(LPC_ETHERNET, true);

#else
Chip_ENET_Init(LPC_ETHERNET, false);
#endif

/* Setup MII clock rate and PHY address */
Chip_ENET_SetupMII(LPC_ETHERNET, Chip_ENET_FindMIIDiv(LPC_ETHERNET, 2500000), 1);

lpc_phy_init(true, localMsDelay);

/* Setup MAC address for device */
Board_ENET_GetMacADDR(macaddr);
Chip_ENET_SetADDR(LPC_ETHERNET, macaddr);

/* Setup descriptors */
InitDescriptors();

/* Enable RX/TX after descriptors are setup */
Chip_ENET_TXEnable(LPC_ETHERNET);
Chip_ENET_RXEnable(LPC_ETHERNET);

while (k) {
/* Check for receive packets */
workbuff = ENET_RXGet(&rxBytes);
if (workbuff) {
/* Packet was received. Dump some info from the packet */
DEBUGOUT("Packet received: ");
ethpkttgl = (bool) !ethpkttgl;

/* Toggle LED2 on each packet received */
Board_LED_Set(1, ethpkttgl);

/* Destination and source MAC addresses */
DEBUGOUT("-Dest MAC: %02x:%02x:%02x:%02x:%02x:%02x-",
 workbuff[0], workbuff[1], workbuff[2], workbuff[3], workbuff[4], workbuff[5]);
DEBUGOUT("-Source MAC: %02x:%02x:%02x:%02x:%02x:%02x-",
 workbuff[6], workbuff[7], workbuff[8], workbuff[9], workbuff[10], workbuff[11]);

/* Length of received packet and embedded len/type */
DEBUGOUT("-Packet len: %d", rxBytes);
DEBUGOUT("-Type: %04x\r\n", ((((uint32_t) workbuff[12]) << 8) | (((uint32_t) workbuff[13]))));
ENET_RXBuffClaim();
}

/* Send a 'dummy' broadcast packet on a keypress. You'll only see this
     if your using a tool such as WireShark and the packet will not have
   a checksum */
if (DEBUGIN() != EOF) {
/* Only if link detected */
if (physts & PHY_LINK_CONNECTED) {
workbuff = ENET_TXBuffGet();
if (workbuff) {
/* Destination is broadcast */
for (i = 0; i < 6; i++) {
workbuff = 0xFF;
}

/* Source is this MAC address */
memcpy(&workbuff[6], macaddr, 6);

/* Size will be 128 bytes (total) */
workbuff[12] = 0;
workbuff[13] = 128;

/* Some dummy data, fill beyond end of packet */
for (i = 0; i < 128; i++) {
workbuff[i + 14] = (uint8_t) (i & 0xFF);
}

ENET_TXQueue(128);
DEBUGOUT("Packet sent! \r\n");
Board_LED_Set(1, true);
}
}
}
if (ENET_IsTXFinish()) {
Board_LED_Set(1, false);
}
/* PHY status state machine, LED on when connected. This function will
   not block. */
physts = lpcPHYStsPoll();

/* Only check for connection state when the PHY status has changed */
if (physts & PHY_LINK_CHANGED) {
if (physts & PHY_LINK_CONNECTED) {
Board_LED_Set(0, true);

/* Set interface speed and duplex */
if(physts & PHY_LINK_FULLDUPLX)
Chip_ENET_SetFullDuplex(LPC_ETHERNET);
else
Chip_ENET_SetHalfDuplex(LPC_ETHERNET);
if(physts & PHY_LINK_SPEED100)
Chip_ENET_Set100Mbps(LPC_ETHERNET);
else
Chip_ENET_Set10Mbps(LPC_ETHERNET);
}
else {
Board_LED_Set(0, false);
}

DEBUGOUT("Link connect status: %d\r\n", ((physts & PHY_LINK_CONNECTED) != 0));
}
}

/* Never returns, for warning only */
return 0;
}

/**
 * @}
 */


description of that program says:

Quote:
Ethernet example

Example description
The ENET example is a simple ethernet application for sending an ethernet
packet via the MAC and displaying received broadcast packets. The MAC example will
listen for all packets on the ethernet and display some stats via UART when a
packet is received. A dummy packet can also be sent out. Wireshark can be used to
view the outgoing packet.

To use the example, connect a serial cable to the board's RS232/UART port and
start a terminal program to monitor the port.  The terminal program on the host
PC should be setup for 115K8N1. For each packet received, the LED will toggle
and the packets source and destination MAC addresses will be displayed with the
packet type. Pressing any key will send a dummy packet.

Special connection requirements
- Embedded Artists' LPC1788 Developer's Kit:
- Embedded Artists' LPC4088 Developer's Kit:
There are no special connection requirements for this example.
- LPCXpresso LPC1769:
Need to connect with base board for using RS232/UART port and Ethernet port.

Build procedures:
Visit the LPCOpen quickstart guides at link "http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quicks..."
to get started building LPCOpen projects.




so if i understand it right I have to connect any UART to pc port and monitor the port. Maybe those strange signs were send because wrong baudrate, i'll check it in a moment.
How can i send packet via MAC?
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Nov 11 05:46:40 MST 2014

Quote: Zahoq
P0[0] TXD3 is connected to my UART-USB converter connected to PC to RXD (i have example for that UART connection, it works fine)
P0[1] RXD3 is connected to UART-USB converter to TXD.
GND of board and converter is connected, so it's not the problem with UART i gues.



Did you try Semihosting already?

How do you setup UART3? Are we talking about LPCOpen?
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Tue Nov 11 05:17:56 MST 2014
P0[0] TXD3 is connected to my UART-USB converter connected to PC to RXD (i have example for that UART connection, it works fine)
P0[1] RXD3 is connected to UART-USB converter to TXD.
GND of board and converter is connected, so it's not the problem with UART i gues.

Ethernet pins:
TD+ of lpcxpresso is connected to white-green ethernet cable
TD- of lpcxpresso is connected to green ethernet cable
RD+ of lpcxpresso is connected to white-orange ethernet cable
RD- of lpcxpresso is connected to orange ethernet cable

Ethernet cable is connected to PC.
I tried also combination:
TD+ of lpcxpresso is connected to white-orange ethernet cable
TD- of lpcxpresso is connected to orange ethernet cable
RD+ of lpcxpresso is connected to white-green ethernet cable
RD- of lpcxpresso is connected to green ethernet cable

Resoult was the same.

With that connection i'm running periph_ethernet example and i'm scaning Serial connection on my PC by using Hercules program to receive information about sent data, and i don't know why it doesn't work like it should :)
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Nov 11 04:47:32 MST 2014

Quote: Zahoq
In description there is no information about what UART should i use.



And what did you connect to UART3 or is it wireless :)

If you don't describe what you are doing, it's not easy to help you...
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Tue Nov 11 04:38:19 MST 2014
Those strange sings are send when LED on LPCXPRESSO blinks which means it sends data packet via ethernet, so it doesn't spam with that sings randomly. In description there is no information about what UART should i use.
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Nov 11 04:19:11 MST 2014

Quote: Zahoq
... but only strange signs. I'm connected to UART3 pins.



So whatever is connected to UART3, that's obviously not working...
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Zahoq on Tue Nov 11 04:11:41 MST 2014
I tried to run periph_ethernet. LEDs on LPCXPRESSO blinks so i gues it's sending something, but i don't know why i don't receive information on UART like "Packet received: " but only strange signs. I'm connected to UART3 pins.
0 件の賞賛
返信

3,833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Nov 10 19:55:09 MST 2014
Hi Zahoq,
Can you please let us know which example are you using?
0 件の賞賛
返信