save on flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

save on flash memory

1,250件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AndreSTB on Fri Jul 13 13:57:47 MST 2012
Hi,

I'm starting to work with LPC4350, and I need to know how save on the external memory the boot program. Anybody have a document that explaning about this or know teach me.

I'm using the LPCXpresso to debug.

Thanks
André Lessa
0 件の賞賛
返信
4 返答(返信)

1,234件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AndreSTB on Thu Jul 19 05:32:24 MST 2012
Hi,

I read the link said in previous post and helped me, but I never used a ARM with external memory and I need a document with more details (Tutorials). If anybody can help me I will be happy.

Thanks
André Lessa
0 件の賞賛
返信

1,234件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jul 17 10:37:59 MST 2012
Did you look at the FAQ that I previously pointed you to??

Regards,
CodeRedSupport
0 件の賞賛
返信

1,234件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AndreSTB on Mon Jul 16 07:06:14 MST 2012
Hi

I need to know what I make to load the program in a external memory of the LPC4350 using the LPCXpresso? Becuse how the LPC4350 don't have a internaly memory flash I need to load in the external memory flash, then I did a bord and put a memory flash on channel SPIFI of the ARM, but I dont know how load the program in this memory.

Thanks
André Lessa
0 件の賞賛
返信

1,234件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Jul 16 01:39:26 MST 2012
Sorry, I'm not sure I follow what you are asking. Can you explain in more detail?

I would also suggest that if you are working with LPC43xx, then you should take a look at the following FAQ:

http://support.code-red-tech.com/CodeRedWiki/LPC1850_4350_Support

Regards,
CodeRed Support
0 件の賞賛
返信