sample code mmc_fat build problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sample code mmc_fat build problem

773件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Olivier on Mon Oct 31 06:19:32 MST 2011
I study the example of mmc_fat of EA baseboard, but it doesn't want to build.

The cr_startup_lpc176x.c file doesn't find ==> system_LPC17xx.h

I think the problem is that i have to include CMSISv2_LPC17xx/inc to include directory?

I don't know to add this directory of h files into the includes-tab??

How it works??
0 件の賞賛
返信
1 返信

766件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Oct 31 06:32:13 MST 2011
This link describes how to change Includes and Libraries:

http://knowledgebase.nxp.com/showthread.php?t=2326
0 件の賞賛
返信