request for help on ir sensor code for lpc1114

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

request for help on ir sensor code for lpc1114

1,817 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vin.8teen on Fri Feb 24 21:18:58 MST 2012
hi ppl,

its a humble request for a simple ir sensor example code for lpc1114

thanku&regards
vinay murthy
0 Kudos
Reply
7 Replies

1,763 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sharif on Sat Jul 19 21:43:55 MST 2014
can any one provide sample IR code  for on and off my AirConditioner
0 Kudos
Reply

1,763 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Wed Feb 05 06:25:31 MST 2014
Just connect the output of the IR sensor to a GPIO and check the level. A high level means something detected a low level means no activity.

Just make sure you stay well into the limits of the GPIO specs.
0 Kudos
Reply

1,763 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stefi on Wed Feb 05 00:26:45 MST 2014
http://learn.adafruit.com/pir-passive-infrared-proximity-motion-sensor/
0 Kudos
Reply

1,763 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Tue Feb 04 01:44:00 MST 2014
Please give us the datasheet of the used ir sensor
0 Kudos
Reply

1,763 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stefi on Fri Jan 31 06:20:15 MST 2014
how can i read simple ir sensor using lpc1343 in lpcxpresso?
please help me ....
0 Kudos
Reply

1,763 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vin.8teen on Mon Mar 12 01:51:25 MST 2012
sir we using a basic ir sensor which is of 935nm wavelength. its just to interface with lpc1114 as an example code. so as to see signal transfer.
0 Kudos
Reply

1,763 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Sat Feb 25 13:26:57 MST 2012
Hello vin.8teen,

what kind of IR-sensor do you use? Opto-coupler ... IR-transistor connected to ground with pull-up resistor.

Or do you mean some received protocol to be translated via the LPCXpresso?
0 Kudos
Reply