problems building LPCOpen projects in LPXCpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problems building LPCOpen projects in LPXCpresso

916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bowerymarc on Wed Apr 10 15:45:47 MST 2013
I've downloaded LPCOpen v1.02, and lpcxpresso_5.1.2_2065, to try to do some SD Benchmarking using the Hitex Eva 4350 board.

I've imported the following projects into my workspace:
lpc18xx_43xx_lib_lpc_board
lpc43xx_hitex_eva_4350_board_lib
lpc43xx_hitex_eva_4350_board_lib_m0
lpc43xx_hitex_eva_4350_periph_sdmmc

On the first library (lpc_board) I selected the hitex_eva_4350 build target.  I'm able to build all 3 libraries with no errors.  But when I build the sdmmc project I get this:


Quote:
18:12:28 **** Incremental Build of configuration Debug for project lpc43xx_hitex_eva_4350_periph_sdmmc ****
make -j4 all
Building file: Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/software/filesystems/fatfslpc/rtc.c
Building file: Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/software/filesystems/fatfslpc/fs_mci.c
Invoking: MCU C Compiler
Invoking: MCU C Compiler
Building file: Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/applications/lpc18xx_43xx/examples/periph/periph_sdmmc/sdmmc.c
arm-none-eabi-gcc -D__REDLIB__ -DDEBUG -D__CODE_RED -DCORE_M4 -I"../../../../../../../software/CMSIS/CMSIS/Include" -I"../../../../../../../software/lpc_core/lpc_ip" -I"../../../../../../../software/filesystems/fatfs/src" -I"../../../../../../../software/filesystems/fatfslpc" -I"../../../../../examples/periph/periph_sdmmc" -I"../../../../../../../software/lpc_core/lpc_chip/chip_18xx_43xx" -I"../../../../../../../software/lpc_core/lpc_chip/chip_common" -I"../../../../../../../software/lpc_core/lpc_board/board_common" -I"../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350" -I"../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350/hitex_eva_4350" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -fsingle-precision-constant -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -mthumb -MMD -MP -MF"fatfs/rtc.d" -MT"fatfs/rtc.d" -o "fatfs/rtc.o" "Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/software/filesystems/fatfslpc/rtc.c"
arm-none-eabi-gcc -D__REDLIB__ -DDEBUG -D__CODE_RED -DCORE_M4 -I"../../../../../../../software/CMSIS/CMSIS/Include" -I"../../../../../../../software/lpc_core/lpc_ip" -I"../../../../../../../software/filesystems/fatfs/src" -I"../../../../../../../software/filesystems/fatfslpc" -I"../../../../../examples/periph/periph_sdmmc" -I"../../../../../../../software/lpc_core/lpc_chip/chip_18xx_43xx" -I"../../../../../../../software/lpc_core/lpc_chip/chip_common" -I"../../../../../../../software/lpc_core/lpc_board/board_common" -I"../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350" -I"../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350/hitex_eva_4350" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -fsingle-precision-constant -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -mthumb -MMD -MP -MF"fs_mci.d" -MT"fs_mci.d" -o "fs_mci.o" "Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/software/filesystems/fatfslpc/fs_mci.c"
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__REDLIB__ -DDEBUG -D__CODE_RED -DCORE_M4 -I"../../../../../../../software/CMSIS/CMSIS/Include" -I"../../../../../../../software/lpc_core/lpc_ip" -I"../../../../../../../software/filesystems/fatfs/src" -I"../../../../../../../software/filesystems/fatfslpc" -I"../../../../../examples/periph/periph_sdmmc" -I"../../../../../../../software/lpc_core/lpc_chip/chip_18xx_43xx" -I"../../../../../../../software/lpc_core/lpc_chip/chip_common" -I"../../../../../../../software/lpc_core/lpc_board/board_common" -I"../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350" -I"../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350/hitex_eva_4350" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -fsingle-precision-constant -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=softfp -mthumb -MMD -MP -MF"sdmmc.d" -MT"sdmmc.d" -o "sdmmc.o" "Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/applications/lpc18xx_43xx/examples/periph/periph_sdmmc/sdmmc.c"
In file included from Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/software/filesystems/fatfslpc/rtc.c:14:0:
../../../../../../../software/lpc_core/lpc_chip/chip_18xx_43xx/chip.h:32:24: fatal error: sys_config.h: No such file or directory
compilation terminated.
make: *** [fatfs/rtc.o] Error 1
make: *** Waiting for unfinished jobs....
In file included from ../../../../../examples/periph/periph_sdmmc/fsmci_cfg.h:43:0,
                 from Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/software/filesystems/fatfslpc/fs_mci.c:32:
../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350/board.h:35:38: fatal error: board_hitex_eva_18504350.h: No such file or directory
compilation terminated.
make: *** [fs_mci.o] Error 1
In file included from Y:/BEA/ioti/software/lpcSDBenchmarking/LPCOpen_v1.02/applications/lpc18xx_43xx/examples/periph/periph_sdmmc/sdmmc.c:33:0:
../../../../../../../software/lpc_core/lpc_board/boards_18xx_43xx/hitex_eva_18504350/board.h:35:38: fatal error: board_hitex_eva_18504350.h: No such file or directory
compilation terminated.
make: *** [sdmmc.o] Error 1

18:12:31 Build Finished (took 2s.437ms)



I get the same errors when trying other projects (e.g. freertos_blinky)

what's really odd is, they compile OK with the OSX version of LPCXpresso, but not the windows one!  (I had to switch because the Keil ULINK2 apparently isn't supported in the OSX version, even though the device is a bog-stock USB HID as far as the OS is concerned and needs no drivers).

Anyone have a clue what's going on??
0 件の賞賛
返信
0 返答(返信)