memory section

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

memory section

1,186 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by johanan on Tue Oct 08 06:35:19 MST 2013
I need a lot of ram variables, and have a large external SDRAM.
How do I set the linker memory sections?
Is there an "easy" way to configure this?
I understand that some linker script must be edited, and a link to a simple explanation will be appreciated.
Thanks
0 Kudos
Reply
4 Replies

1,173 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by johanan on Tue Oct 08 23:28:35 MST 2013
I would like to use Xpersso, currently using Crossworks, with emWin.

I am just too used to auto completion, which is makes Rowley Crossworks looks like an outdated IDE, otherwise it is quite good.

( Is there a way to transfer Crossworks project to LPCXpresso? both are GNU tools...)

0 Kudos
Reply

1,173 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by johanan on Tue Oct 08 23:23:37 MST 2013
Thank you  :)
0 Kudos
Reply

1,173 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Tue Oct 08 08:51:58 MST 2013
Are you using emwin? Which IDE you're using?
0 Kudos
Reply

1,173 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Oct 08 06:56:28 MST 2013
http://support.code-red-tech.com/CodeRedWiki/EnhancedManagedLinkScripts
0 Kudos
Reply