malloc.h vs Redlib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

malloc.h vs Redlib

1,333 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Marco72 on Mon Nov 21 22:57:32 MST 2011
Using LPCXpresso v4.0.5 [Build 123] [27/06/2011] with a LPC1769 rev b board I encountered a problem when in my code i write this include

#include <malloc.h>


if I switch to newlib the problem disappears.

Follow the last stage of fail build from console window:

Building file: ../src/main.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__REDLIB__ -DDEBUG -D__CODE_RED -D__USE_CMSIS=CMSISv2p00_LPC17xx -I"C:\Documenti\Progetti\Miei\LPC expresso\USB\Test\CMSISv2p00_LPC17xx\inc" -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"src/main.d" -MT"src/main.d" -o"src/main.o" "../src/main.c"
In file included from ../src/main.c:24:0:
c:\nxp\lpcxpresso_4.0.5_123\lpcxpresso\tools\bin\../lib/gcc/arm-none-eabi/4.5.1/../../../../arm-none-eabi/include/malloc.h:4:29: error: no include path in which to search for malloc.h
make: *** [src/main.o] Error 1

To understand what happen I made a completely new LPCXpresso empty project using the provided wizard and this is always the behaviour.

Where is my error ?  Does malloc.h is supported in Redlib ?
Looking at include path I am a bit confused:
In project tree I see under the includes branch some .h yellow folders (where path is within lpcxpresso installation include folders) and an other violet folder that is derived from my project setting. How these paths are managed during build process?

Thank you

Marco
0 Kudos
Reply
1 Reply

1,250 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ecw on Tue Nov 22 02:57:28 MST 2011
Ignore it.  Use stdlib.h instead.  malloc.h is deprecated, and disappearing from many systems.
:confused:
0 Kudos
Reply