make: *** Error 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

make: *** Error 1

893件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drvrh on Mon Jul 13 22:12:13 MST 2015
Hello,

I create project and run, project debug normal and working, when I add something .h file and one more .c file not working and I get error:

make: *** [src/cr_startup_lpc175xx_6xx.o] Erro 1

What I doin'g wrong?

0 件の賞賛
返信
1 返信

879件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 14 00:17:40 MST 2015
That's just make reporting there was an error. Look through the build log (or in the Problems view) to see what the actual details of the error are.

https://www.lpcware.com/content/faq/lpcxpresso/build-console

Then fix it!

Regards,
LPCXpresso Support
0 件の賞賛
返信