lpc1764 + lan8720a, problem with packets

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc1764 + lan8720a, problem with packets

5,418 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Tue Nov 27 07:58:20 MST 2012
Hi,

I'm running uIP example on my own pcb with lpc1764 and lan8720a. When I send packets via ethernet from uC to PC everything is fine, but in the other direction packets are distorted, eg:

PC sends:
ff ff ff ff ff ff bc ae  c5 16 eb 89 08 06 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00

uC gets:
ff ff ff ff ff 7f bc 2e  c5 14 6b 01 00 04 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 a4 4b d2

another,
PC sends:
ff ff ff ff ff ff ff ff  ff ff ff ff 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 

uC gets:
ff ff ff ff ff ff ff ff  ff ff ff 7f 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00  00 00 00 00 04 55 14

Does anyone know what can be wrong?
0 Kudos
Reply
23 Replies

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Dec 06 01:54:12 MST 2012

Quote: rasiak
Are receiving bytes also correct? Can You check it with wireshark?


My Ethernet Frame (UDP broadcast) is shown as it is sent and also as Wireshark is showing it. Therefore I decided that it's working ;)


Quote: rasiak
Not yet, but I think I will have to... is there any chance to get it working without this?



Don't know that. All schematics I've seen include this inverter and  so I think it's necessary. I don't know why your CAD designer didn't  include it, but perhaps he knows more than we and can enlighten you :rolleyes:
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Thu Dec 06 01:28:41 MST 2012

Quote:
This sample is working incredible slow, but correct with my  LPCXpresso1769 (12MHz crystal / 100MHz main clock) &  LAN8720(25MHz)  and my CMSIS2.0 (with standard setting) :)

Are receiving bytes also correct? Can You check it with wireshark?
and one more thing :) it's doesn't work and crash when I'm trying to change speed of my MAC card to 10mbit/s..


Quote:
Did you add the inverter meanwhile?

Not yet, but I think I will have to... is there any chance to get it working without this?
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Dec 05 17:35:57 MST 2012
This sample is working incredible slow, but correct with my LPCXpresso1769 (12MHz crystal / 100MHz main clock) &  LAN8720(25MHz) and my CMSIS2.0 (with standard setting) :)

Don't know what you have changed in CMSIS except oscillator and PLL setting, but I would strongly recommend to use CLKOUT and scope main clock to ensure a correct speed.

Did you add the inverter meanwhile?

To exclude a few potential problems I would also test a standard CMSIS with 12MHz crystal.

If you want to speed up your incredible slow semihosting, you can use itoa to convert your bytes to hex ascii, add this to a char array and then printf this array.

That's much faster then printf every byte of your buffer  ;)
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Wed Dec 05 17:09:18 MST 2012
PHY has 25mhz crystal connected to XTAL1 and XTAL2(just like on 35th page of datasheet http://www.smsc.com/media/Downloads_Public/Data_Sheets/8720a.pdf), crystal for uC has 8mhz.. Is that what You mean?
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Dec 05 16:17:07 MST 2012

Quote: Zero
Which crystal are you using und which main clock are you trying to generate :confused:



I'm still missing your clock data :(
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Wed Dec 05 16:13:06 MST 2012

Quote:
You're kidding :) EMAC init isn't working because of  wrong LAN8720_DEF_ADR
Who has mutilated this? Use correct:
     Code:
      #define LAN8720_DEF_ADR        0x0100

It's not workning, on my pcb PHYADR is 0 :D


Quote:
Your included CMSIS1.3 is awful :mad: Use new CMSIS2.0.

As You wish ;): [ATTACH]898[/ATTACH]
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Dec 05 12:02:08 MST 2012

Quote: rasiak
ok, you're right this is better version



You're kidding EMAC init isn't working because of  wrong LAN8720_DEF_ADR :mad:

Who has mutilated this? Use correct:
 #define LAN8720_DEF_ADR        0x0100

Quote: rasiak
still not working(errors in some bits), could you  run this?



No, I can't. Your included CMSIS1.3 is awful :mad: Use new CMSIS2.0. Which crystal are you using und which main clock are you trying to generate.

I think your main problem is your cheesy clock setup :eek:
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Tue Dec 04 15:00:12 MST 2012

Quote: rasiak
ps. on my pcb there is no inverter on REFCLK pin(LAN8720), is it necessary?? (RDB1768 DEVELOPMENT BOARD has it)


I remarked that it was necessary, when I was building my LPC1764 board.

Although I have seen some designs that do not include it.

Edit: Oh, my board is available again, now 3!!!
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Tue Dec 04 14:52:04 MST 2012
ok, you're right :/ this is better version [ATTACH]897[/ATTACH], still not working(errors in some bits), could you run this?
ps. on my pcb there is no inverter on REFCLK pin(LAN8720), is it necessary?? (RDB1768 DEVELOPMENT BOARD has it)
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Dec 02 15:49:20 MST 2012
Obviously you are not running LAN8720 Code in your EMAC_Init :mad:

That's no link check, that's an autonegotiate check (which was already done before) :confused:
  /* Check the link status. */
  for (tout = 0; tout < 0x10000; tout++) {
    regv = read_PHY (PHY_REG_PHY_CTRL);
    if (regv & PHY_AUTO_NEG_COMPLETE)
    {       
      /* Link is on. */
        printf("Link is on\n");
      break;
    }
  } 
A correct link test is:
  // Now check the link status LAN
   value = udp_readPHY (PHY_REG_BMSR);
   if (value & 0x0004)
   {
// The link is on
    break;
   } 
Also Duplex reading is wrong:
 if (regv & PHY_SPEED_FDUPLX)
  {
    /* Full duplex is enabled. */
      printf("full duplex\n");
      LPC_EMAC->MAC2    |= MAC2_FULL_DUP;
      LPC_EMAC->Command |= CR_FULL_DUP;
      LPC_EMAC->IPGT     = IPGT_FULL_DUP;
  }
  else {
    /* Half duplex mode. */
      printf("half duplex\n");
      LPC_EMAC->IPGT = IPGT_HALF_DUP;
Correct Duplex reading is:
 value = udp_readPHY(PHY_REG_SPECIAL);
// Now configure for full/half duplex mode
  if (value & 0b10000)
  {
// We are in full duplex is enabled mode
   LPC_EMAC->MAC2    |= MAC2_FULL_DUP;
   LPC_EMAC->Command |= CR_FULL_DUP;
   LPC_EMAC->IPGT     = IPGT_FULL_DUP;
  }
  else
  {
// Otherwise we are in half duplex mode
   LPC_EMAC->IPGT = IPGT_HALF_DUP;
  }
Speed reading is wrong:
 /* Configure 100MBit/10MBit mode. */
  if (!(regv & PHY_SPEED_100))
  {
    /* 10MBit mode. */
      printf("10mbit\n");
      LPC_EMAC->SUPP = 0;
  }
  else {
    /* 100MBit mode. */
      printf("100mbit\n");
      LPC_EMAC->SUPP = SUPP_SPEED;
  }
Correct reading is:
 value = udp_readPHY(PHY_REG_SPECIAL);
...
// Now configure 100MBit or 10MBit mode
  if (value & 0b01000)
  {
// 100MBit mode
   LPC_EMAC->SUPP = SUPP_SPEED;
  }
  else
  {
// 10MBit mode
   LPC_EMAC->SUPP = 0;
  }
 } 
[B][COLOR=Red]So whatever you init, it's not a LAN8720[/COLOR][/B] (http://www.smsc.com/media/Downloads_Public/Data_Sheets/8720a.pdf)  :eek:
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Sun Dec 02 14:07:06 MST 2012
This is my code packed in one zip file... [ATTACH]896[/ATTACH]
If someone could test it with lpc17xx and lan8720, it would be great :rolleyes:
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yanvasilij on Fri Nov 30 04:20:42 MST 2012
In some boards there is problem with  schematics like this www.utasker.com/forum/index.php?topic=579.5;wap2. It occur crc-error.
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Thu Nov 29 17:05:20 MST 2012

Quote:
Perhaps you want to export and post your complete project so someone can test it with a standard 1768 & LAN8720 ;)



Actually I would be happy if someone who already did ethernet connection could check this code and give me an advice what to change :rolleyes:
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Nov 29 12:17:01 MST 2012

Quote: rasiak
i've checked signals between lan8720 and lpc1764 and it looks fine(bytes are correct), so uC is faulty..


:confused: Sorry, can't  follow you.

Perhaps you want to export and post your complete project so someone can test it with a standard 1768 & LAN8720 ;)
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Thu Nov 29 11:22:07 MST 2012
lpc17xx_emac.h

...
/* LAN8720 PHY Registers */ 
#define PHY_REG_BMCR        0x00        /* Basic Mode Control Register       */ 
#define PHY_REG_BMSR        0x01        /* Basic Mode Status Register        */ 
#define PHY_REG_IDR1        0x02        /* PHY Identifier 1                  */ 
#define PHY_REG_IDR2        0x03        /* PHY Identifier 2                  */ 
#define PHY_REG_ANAR        0x04        /* Auto-Negotiation Advertisement    */ 
#define PHY_REG_ANLPAR      0x05        /* Auto-Neg. Link Partner Abitily    */ 
#define PHY_REG_ANER        0x06        /* Auto-Neg. Expansion Register      */ 
 
/* PHY Extended Registers */ 
#define    PHY_REG_MODE_CTRL        17 
#define    PHY_REG_SPECIAL_MODE    18 
#define    PHY_REG_SYMBOL_ERR_CNT    26 
#define    PHY_REG_SPECIAL_CTRL    27 
#define    PHY_REG_INT_SOURCE        29 
#define    PHY_REG_INT_MASK        30 
#define    PHY_REG_PHY_CTRL        31 
 
#define PHY_FULLD_100M      0x2100      /* Full Duplex 100Mbit               */ 
#define PHY_HALFD_100M      0x2000      /* Half Duplex 100Mbit               */ 
#define PHY_FULLD_10M       0x0100      /* Full Duplex 10Mbit                */ 
#define PHY_HALFD_10M       0x0000      /* Half Duplex 10MBit                */ 
#define PHY_AUTO_NEG        0x3000      /* Select Auto Negotiation           */ 
//#define PHY_AUTO_NEG_COMPLETE 0x0020    /* Auto negotiation have finished.   */ 
 
 
 
//#define PHY_AUTO_NEG            0x3000  /* Select Auto Negotiation           */ 
#define PHY_AUTO_NEG_COMPLETE     0x1000    /* Auto negotiation have finished.   */ 
#define PHY_SPEED_FDUPLX         0x0010    /* Full Duplex   */ 
#define PHY_SPEED_100             0x0008    /* 100Mbit   */ 
 
#define LAN8720_DEF_ADR        0x0100      /* Default PHY device address        */ 
#define LAN8720_ID          0x0007C0F0  /* PHY Identifier                    */ 
#else 
    #error "No board" 
#endif 
 
#endif
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Thu Nov 29 11:19:39 MST 2012
system_LPC17xx.c
 
  #include <stdint.h> 
  #include "LPC17xx.h" 
   
  #define CLOCK_SETUP           1 
  #define SCS_Val               0x00000020 
  #define CLKSRCSEL_Val         0x00000001 
  #define PLL0_SETUP            1 
  #define PLL0CFG_Val           0x00000018 // 100MHz //0x00110132 
  #define PLL1_SETUP            1 
  #define PLL1CFG_Val           0x00000023 
  #define CCLKCFG_Val           0x00000003 
  #define USBCLKCFG_Val         0x00000000 
  #define PCLKSEL0_Val          0x00000000 
  #define PCLKSEL1_Val          0x00000000 
  #define PCONP_Val             0x042887DE 
  #define CLKOUTCFG_Val         0x00000000 
  
  // 
  // <e> Flash Accelerator Configuration 
  //   <o1.12..15> FLASHTIM: Flash Access Time 
  //               <0=> 1 CPU clock (for CPU clock up to 20 MHz) 
  //               <1=> 2 CPU clocks (for CPU clock up to 40 MHz) 
  //               <2=> 3 CPU clocks (for CPU clock up to 60 MHz) 
  //               <3=> 4 CPU clocks (for CPU clock up to 80 MHz) 
  //               <4=> 5 CPU clocks (for CPU clock up to 100 MHz) 
  //               <5=> 6 CPU clocks (for any CPU clock) 
  // </e> 
  */ 
  #define FLASH_SETUP           1 //1 
  #define FLASHCFG_Val          0x00004000 

   
  /*---------------------------------------------------------------------------- 
    Check the register settings 
   *----------------------------------------------------------------------------*/ 
  #define CHECK_RANGE(val, min, max)                ((val < min) || (val > max)) 
  #define CHECK_RSVD(val, mask)                     (val & mask) 
   
  /* Clock Configuration -------------------------------------------------------*/ 
  #if (CHECK_RSVD((SCS_Val),       ~0x00000030)) 
     #error "SCS: Invalid values of reserved bits!" 
  #endif 
   
  #if (CHECK_RANGE((CLKSRCSEL_Val), 0, 2)) 
     #error "CLKSRCSEL: Value out of range!" 
  #endif 
   
  #if (CHECK_RSVD((PLL0CFG_Val),   ~0x00FF7FFF)) 
     #error "PLL0CFG: Invalid values of reserved bits!" 
  #endif 
   
  #if (CHECK_RSVD((PLL1CFG_Val),   ~0x0000007F)) 
     #error "PLL1CFG: Invalid values of reserved bits!" 
  #endif 
   
  #if (PLL0_SETUP)            /* if PLL0 is used */ 
    #if (CCLKCFG_Val < 2)     /* CCLKSEL must be greater then 1 */ 
      #error "CCLKCFG: CCLKSEL must be greater then 1 if PLL0 is used!" 
    #endif 
  #endif 
   
  #if (CHECK_RANGE((CCLKCFG_Val), 2, 255)) 
     #error "CCLKCFG: Value out of range!" 
  #endif 
   
  #if (CHECK_RSVD((USBCLKCFG_Val), ~0x0000000F)) 
     #error "USBCLKCFG: Invalid values of reserved bits!" 
  #endif 
   
  #if (CHECK_RSVD((PCLKSEL0_Val),   0x000C0C00)) 
     #error "PCLKSEL0: Invalid values of reserved bits!" 
  #endif 
   
  #if (CHECK_RSVD((PCLKSEL1_Val),   0x03000300)) 
     #error "PCLKSEL1: Invalid values of reserved bits!" 
  #endif 
   
  #if (CHECK_RSVD((PCONP_Val),      0x10100821)) 
     #error "PCONP: Invalid values of reserved bits!" 
  #endif 
   
  #if (CHECK_RSVD((CLKOUTCFG_Val), ~0x000001FF)) 
     #error "CLKOUTCFG: Invalid values of reserved bits!" 
  #endif 
   
  /* Flash Accelerator Configuration -------------------------------------------*/ 
  #if (CHECK_RSVD((FLASHCFG_Val), ~0x0000F000)) 
     #error "FLASHCFG: Invalid values of reserved bits!" 
  #endif 
   
   
  /*---------------------------------------------------------------------------- 
    DEFINES 
   *----------------------------------------------------------------------------*/ 
       
  /*---------------------------------------------------------------------------- 
    Define clocks 
   *----------------------------------------------------------------------------*/ 
  #define XTAL        (8000000UL)        /* Oscillator frequency               */ 
  #define OSC_CLK     (      XTAL)        /* Main oscillator frequency          */ 
  #define RTC_CLK     (   32000UL)        /* RTC oscillator frequency           */ 
  #define IRC_OSC     ( 4000000UL)        /* Internal RC oscillator frequency   */ 
   
   
  /* F_cco0 = (2 * M * F_in) / N  */ 
  #define __M               (((PLL0CFG_Val      ) & 0x7FFF) + 1) 
  #define __N               (((PLL0CFG_Val >> 16) & 0x00FF) + 1) 
  #define __FCCO(__F_IN)    ((2 * __M * __F_IN) / __N)  
  #define __CCLK_DIV        (((CCLKCFG_Val      ) & 0x00FF) + 1) 
   
  /* Determine core clock frequency according to settings */ 
   #if (PLL0_SETUP) 
      #if   ((CLKSRCSEL_Val & 0x03) == 1) 
          #define __CORE_CLK (__FCCO(OSC_CLK) / __CCLK_DIV) 
      #elif ((CLKSRCSEL_Val & 0x03) == 2) 
          #define __CORE_CLK (__FCCO(RTC_CLK) / __CCLK_DIV) 
      #else  
          #define __CORE_CLK (__FCCO(IRC_OSC) / __CCLK_DIV) 
      #endif 
   #else 
      #if   ((CLKSRCSEL_Val & 0x03) == 1) 
          #define __CORE_CLK (OSC_CLK         / __CCLK_DIV) 
      #elif ((CLKSRCSEL_Val & 0x03) == 2) 
          #define __CORE_CLK (RTC_CLK         / __CCLK_DIV) 
      #else 
          #define __CORE_CLK (IRC_OSC         / __CCLK_DIV) 
      #endif 
   #endif 
   
   
  /*---------------------------------------------------------------------------- 
    Clock Variable definitions 
   *----------------------------------------------------------------------------*/ 
  uint32_t SystemCoreClock = __CORE_CLK;/*!< System Clock Frequency (Core Clock)*/ 
   
   
  /*------------------------------------------------
    Clock functions 
   *----------------------------------------------------------------------------*/ 
  void SystemCoreClockUpdate (void)            /* Get Core Clock Frequency      */ 
  { 
    /* Determine clock frequency according to clock register values             */ 
    if (((LPC_SC->PLL0STAT >> 24) & 3) == 3) { /* If PLL0 enabled and connected */ 
      switch (LPC_SC->CLKSRCSEL & 0x03) { 
        case 0:                                /* Int. RC oscillator => PLL0    */ 
        case 3:                                /* Reserved, default to Int. RC  */ 
          SystemCoreClock = (IRC_OSC *  
                            ((2 * ((LPC_SC->PLL0STAT & 0x7FFF) + 1)))  / 
                            (((LPC_SC->PLL0STAT >> 16) & 0xFF) + 1)    / 
                            ((LPC_SC->CCLKCFG & 0xFF)+ 1)); 
          break; 
        case 1:                                /* Main oscillator => PLL0       */ 
          SystemCoreClock = (OSC_CLK *  
                            ((2 * ((LPC_SC->PLL0STAT & 0x7FFF) + 1)))  / 
                            (((LPC_SC->PLL0STAT >> 16) & 0xFF) + 1)    / 
                            ((LPC_SC->CCLKCFG & 0xFF)+ 1)); 
          break; 
        case 2:                                /* RTC oscillator => PLL0        */ 
          SystemCoreClock = (RTC_CLK *  
                            ((2 * ((LPC_SC->PLL0STAT & 0x7FFF) + 1)))  / 
                            (((LPC_SC->PLL0STAT >> 16) & 0xFF) + 1)    / 
                            ((LPC_SC->CCLKCFG & 0xFF)+ 1)); 
          break; 
      } 
    } else { 
      switch (LPC_SC->CLKSRCSEL & 0x03) { 
        case 0:                                /* Int. RC oscillator => PLL0    */ 
        case 3:                                /* Reserved, default to Int. RC  */ 
          SystemCoreClock = IRC_OSC / ((LPC_SC->CCLKCFG & 0xFF)+ 1); 
          break; 
        case 1:                                /* Main oscillator => PLL0       */ 
          SystemCoreClock = OSC_CLK / ((LPC_SC->CCLKCFG & 0xFF)+ 1); 
          break; 
        case 2:                                /* RTC oscillator => PLL0        */ 
          SystemCoreClock = RTC_CLK / ((LPC_SC->CCLKCFG & 0xFF)+ 1); 
          break; 
      } 
    } 
   
  } 
   
  
  void SystemInit (void) 
  { 
  #if (CLOCK_SETUP)                       /* Clock Setup                        */ 
    LPC_SC->SCS       = SCS_Val; 
    if (SCS_Val & (1 << 5)) {             /* If Main Oscillator is enabled      */ 
      while ((LPC_SC->SCS & (1<<6)) == 0);/* Wait for Oscillator to be ready    */ 
    } 
   
    LPC_SC->CCLKCFG   = CCLKCFG_Val;      /* Setup Clock Divider                */ 
   
    LPC_SC->PCLKSEL0  = PCLKSEL0_Val;     /* Peripheral Clock Selection         */ 
    LPC_SC->PCLKSEL1  = PCLKSEL1_Val; 
   
    LPC_SC->CLKSRCSEL = CLKSRCSEL_Val;    /* Select Clock Source for PLL0       */ 
   
  #if (PLL0_SETUP) 
    LPC_SC->PLL0CFG   = PLL0CFG_Val;      /* configure PLL0                     */ 
    LPC_SC->PLL0FEED  = 0xAA; 
    LPC_SC->PLL0FEED  = 0x55; 
   
    LPC_SC->PLL0CON   = 0x01;             /* PLL0 Enable                        */ 
    LPC_SC->PLL0FEED  = 0xAA; 
    LPC_SC->PLL0FEED  = 0x55; 
    while (!(LPC_SC->PLL0STAT & (1<<26)));/* Wait for PLOCK0                    */ 
   
    LPC_SC->PLL0CON   = 0x03;             /* PLL0 Enable & Connect              */ 
    LPC_SC->PLL0FEED  = 0xAA; 
    LPC_SC->PLL0FEED  = 0x55; 
    while (!(LPC_SC->PLL0STAT & ((1<<25) | (1<<24))));/* Wait for PLLC0_STAT & PLLE0_STAT */ 
  #endif 
   
  #if (PLL1_SETUP) 
    LPC_SC->PLL1CFG   = PLL1CFG_Val; 
    LPC_SC->PLL1FEED  = 0xAA; 
    LPC_SC->PLL1FEED  = 0x55; 
   
    LPC_SC->PLL1CON   = 0x01;             /* PLL1 Enable                        */ 
    LPC_SC->PLL1FEED  = 0xAA; 
    LPC_SC->PLL1FEED  = 0x55; 
    while (!(LPC_SC->PLL1STAT & (1<<10)));/* Wait for PLOCK1                    */ 
   
    LPC_SC->PLL1CON   = 0x03;             /* PLL1 Enable & Connect              */ 
    LPC_SC->PLL1FEED  = 0xAA; 
    LPC_SC->PLL1FEED  = 0x55; 
    while (!(LPC_SC->PLL1STAT & ((1<< 9) | (1<< 8))));/* Wait for PLLC1_STAT & PLLE1_STAT */ 
  #else 
    LPC_SC->USBCLKCFG = USBCLKCFG_Val;    /* Setup USB Clock Divider            */ 
  #endif 
   
    LPC_SC->PCONP     = PCONP_Val;        /* Power Control for Peripherals      */ 
   
    LPC_SC->CLKOUTCFG = CLKOUTCFG_Val;    /* Clock Output Configuration         */ 
  #endif 
   
  #if (FLASH_SETUP == 1)                  /* Flash Accelerator Setup            */ 
    LPC_SC->FLASHCFG  = (LPC_SC->FLASHCFG & ~0x0000F000) | FLASHCFG_Val; 
  #endif 
  }
  
uC is set on 100Mhz, is it enough??
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Thu Nov 29 11:15:56 MST 2012
lpc17xx_emac.c
// ********************************************************************* 
// Define the IP address to be used for the MCU running the TCP/IP stack 
// ********************************************************************* 
#define MYIP_1    192 
#define MYIP_2    168 
#define MYIP_3    0 
#define MYIP_4    100 
 
 
#include "LPC17xx.h" 
 
#include "timer.h" 
#include "uip.h" 
#include "uip_arp.h" 
#include "tapdev.h" 
 
#include <cr_section_macros.h> 
#include <NXP/crp.h> 
// Variable to store CRP value in. Will be placed automatically 
// by the linker when "Enable Code Read Protect" selected. 
// See crp.h header for more information 
__CRP const unsigned int CRP_WORD = CRP_NO_CRP ; 
 
#define BUF ((struct uip_eth_hdr *)&uip_buf[0]) 
 
void uip_log(char *m) 
{ 
  //printf("uIP log message: %s\n", m); 
} 
 
char ipstring [20]; 
 
int main(void) 
{ 
    unsigned int i; 
    uip_ipaddr_t ipaddr;    /* local IP address */ 
    struct timer periodic_timer, arp_timer; 
 
    // Code Red - if CMSIS is being used, then SystemInit() routine 
    // will be called by startup code rather than in application's main() 
//#ifndef __USE_CMSIS 
    // system init 
    SystemInit();    /* setup core clocks */ 
    printf("systemInit"); 
//#endif 
 
    // clock init 
    clock_init(); 
        // two timers for tcp/ip 
    timer_set(&periodic_timer, CLOCK_SECOND / 2); /* 0.5s */ 
    timer_set(&arp_timer, CLOCK_SECOND * 10);    /* 10s */ 
     
    // ethernet init 
    tapdev_init(); 
 
    // Initialize the uIP TCP/IP stack. 
//    uip_init(); 
 
//    uip_ipaddr(ipaddr, MYIP_1,MYIP_2,MYIP_3,MYIP_4); 
//    uip_sethostaddr(ipaddr);    /* host IP address */ 
//    uip_ipaddr(ipaddr, MYIP_1,MYIP_2,MYIP_3,1); 
//    uip_setdraddr(ipaddr);    /* router IP address */ 
//    uip_ipaddr(ipaddr, 255,255,255,0); 
//    uip_setnetmask(ipaddr);    /* mask */ 
 
    // Initialize the HTTP server, listen to port 80. 
    httpd_init(); 
printf("httpd_init"); 
 
SystemCoreClockUpdate (); 
printf("SystemCoreClock: %d\n", SystemCoreClock); 
 
int abc=0; 
    while(1) 
    { 
     /* receive packet and put in uip_buf */ 
        uip_len = tapdev_read(uip_buf); 
        if(uip_len > 0)        /* received packet */ 
        {  
            printf("pakiet "); 
            for(abc=0;abc<uip_len;abc++)printf("%x ",uip_buf[abc]); 
            printf("\n"); 
 
//--------------------------------------------- 
            tapdev_send(uip_buf,uip_len); 
            tapdev_send("jakis tekst ktory ma sprwadzic dzialanie przesylania danych po porcie ethernet",78); 
//----------------------------------------- 
              if(BUF->type == htons(UIP_ETHTYPE_IP))    /* IP packet */ 
              { 
                  printf("IP"); 
                  uip_arp_ipin();     
                  uip_input(); 
                  /* If the above function invocation resulted in data that 
                     should be sent out on the network, the global variable 
                     uip_len is set to a value > 0. */ 
  
                  if(uip_len > 0) 
                { 
                      uip_arp_out(); 
                    tapdev_send(uip_buf,uip_len); 
                  } 
              } 
              else if(BUF->type == htons(UIP_ETHTYPE_ARP))    /*ARP packet */ 
              { 
                  printf("ARP"); 
                uip_arp_arpin(); 
                  /* If the above function invocation resulted in data that 
                     should be sent out on the network, the global variable 
                     uip_len is set to a value > 0. */ 
                  if(uip_len > 0) 
                { 
                    tapdev_send(uip_buf,uip_len);    /* ARP ack*/ 
                  } 
              } 
        } 
        else if(timer_expired(&periodic_timer))    /* no packet but periodic_timer time out (0.5s)*/ 
        { 
              timer_reset(&periodic_timer); 
       
              for(i = 0; i < UIP_CONNS; i++) 
              { 
                  uip_periodic(i); 
                /* If the above function invocation resulted in data that 
                   should be sent out on the network, the global variable 
                   uip_len is set to a value > 0. */ 
                if(uip_len > 0) 
                { 
                  uip_arp_out(); 
                  tapdev_send(uip_buf,uip_len); 
                } 
              } 
#if UIP_UDP 
            for(i = 0; i < UIP_UDP_CONNS; i++) { 
                uip_udp_periodic(i); 
                /* If the above function invocation resulted in data that 
                   should be sent out on the network, the global variable 
                   uip_len is set to a value > 0. */ 
                if(uip_len > 0) { 
                  uip_arp_out(); 
                  tapdev_send(); 
                } 
            } 
#endif /* UIP_UDP */ 
             /* Call the ARP timer function every 10 seconds. */ 
            if(timer_expired(&arp_timer)) 
            { 
                //timer_reset(&arp_timer); 
                //uip_arp_timer(); 
            } 
        } 
    } 
}
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Thu Nov 29 11:15:05 MST 2012
main.c
#define MYIP_1    192 
#define MYIP_2    168 
#define MYIP_3    0 
#define MYIP_4    100 
 
 
#include "LPC17xx.h" 
 
#include "timer.h" 
#include "uip.h" 
#include "uip_arp.h" 
#include "tapdev.h" 
 
#include <cr_section_macros.h> 
#include <NXP/crp.h> 
// Variable to store CRP value in. Will be placed automatically 
// by the linker when "Enable Code Read Protect" selected. 
// See crp.h header for more information 
__CRP const unsigned int CRP_WORD = CRP_NO_CRP ; 
 
#define BUF ((struct uip_eth_hdr *)&uip_buf[0]) 
 
void uip_log(char *m) 
{ 
  //printf("uIP log message: %s\n", m); 
} 
 
char ipstring [20]; 
 
int main(void) 
{ 
    unsigned int i; 
    uip_ipaddr_t ipaddr;    /* local IP address */ 
    struct timer periodic_timer, arp_timer; 
 
    // Code Red - if CMSIS is being used, then SystemInit() routine 
    // will be called by startup code rather than in application's main() 
//#ifndef __USE_CMSIS 
    // system init 
    SystemInit();    /* setup core clocks */ 
    printf("systemInit"); 
//#endif 
 
    // clock init 
    clock_init(); 
        // two timers for tcp/ip 
    timer_set(&periodic_timer, CLOCK_SECOND / 2); /* 0.5s */ 
    timer_set(&arp_timer, CLOCK_SECOND * 10);    /* 10s */ 
     
    // ethernet init 
    tapdev_init(); 
 
    // Initialize the uIP TCP/IP stack. 
//    uip_init(); 
 
//    uip_ipaddr(ipaddr, MYIP_1,MYIP_2,MYIP_3,MYIP_4); 
//    uip_sethostaddr(ipaddr);    /* host IP address */ 
//    uip_ipaddr(ipaddr, MYIP_1,MYIP_2,MYIP_3,1); 
//    uip_setdraddr(ipaddr);    /* router IP address */ 
//    uip_ipaddr(ipaddr, 255,255,255,0); 
//    uip_setnetmask(ipaddr);    /* mask */ 
 
    // Initialize the HTTP server, listen to port 80. 
    httpd_init(); 
printf("httpd_init"); 
 
SystemCoreClockUpdate (); 
printf("SystemCoreClock: %d\n", SystemCoreClock); 
 
int abc=0; 
    while(1) 
    { 
     /* receive packet and put in uip_buf */ 
        uip_len = tapdev_read(uip_buf); 
        if(uip_len > 0)        /* received packet */ 
        {  
            printf("pakiet "); 
            for(abc=0;abc<uip_len;abc++)printf("%x ",uip_buf[abc]); 
            printf("\n"); 
 
//--------------------------------------------- 
            tapdev_send(uip_buf,uip_len); 
            tapdev_send("jakis tekst ktory ma sprwadzic dzialanie przesylania danych po porcie ethernet",78); 
//----------------------------------------- 
              if(BUF->type == htons(UIP_ETHTYPE_IP))    /* IP packet */ 
              { 
                  printf("IP"); 
                  uip_arp_ipin();     
                  uip_input(); 
                  /* If the above function invocation resulted in data that 
                     should be sent out on the network, the global variable 
                     uip_len is set to a value > 0. */ 
  
                  if(uip_len > 0) 
                { 
                      uip_arp_out(); 
                    tapdev_send(uip_buf,uip_len); 
                  } 
              } 
              else if(BUF->type == htons(UIP_ETHTYPE_ARP))    /*ARP packet */ 
              { 
                  printf("ARP"); 
                uip_arp_arpin(); 
                  /* If the above function invocation resulted in data that 
                     should be sent out on the network, the global variable 
                     uip_len is set to a value > 0. */ 
                  if(uip_len > 0) 
                { 
                    tapdev_send(uip_buf,uip_len);    /* ARP ack*/ 
                  } 
              } 
        } 
        else if(timer_expired(&periodic_timer))    /* no packet but periodic_timer time out (0.5s)*/ 
        { 
              timer_reset(&periodic_timer); 
       
              for(i = 0; i < UIP_CONNS; i++) 
              { 
                  uip_periodic(i); 
                /* If the above function invocation resulted in data that 
                   should be sent out on the network, the global variable 
                   uip_len is set to a value > 0. */ 
                if(uip_len > 0) 
                { 
                  uip_arp_out(); 
                  tapdev_send(uip_buf,uip_len); 
                } 
              } 
#if UIP_UDP 
            for(i = 0; i < UIP_UDP_CONNS; i++) { 
                uip_udp_periodic(i); 
                /* If the above function invocation resulted in data that 
                   should be sent out on the network, the global variable 
                   uip_len is set to a value > 0. */ 
                if(uip_len > 0) { 
                  uip_arp_out(); 
                  tapdev_send(); 
                } 
            } 
#endif /* UIP_UDP */ 
             /* Call the ARP timer function every 10 seconds. */ 
            if(timer_expired(&arp_timer)) 
            { 
                //timer_reset(&arp_timer); 
                //uip_arp_timer(); 
            } 
        } 
    } 
}
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rasiak on Thu Nov 29 10:30:08 MST 2012
no, i don't have another board..
i've checked signals between lan8720 and lpc1764 and it looks fine(bytes are correct), so uC is faulty..
0 Kudos
Reply

5,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Nov 29 07:15:46 MST 2012
Did you try your Code with another (not own PCB) board already to exclude hardware problems?
0 Kudos
Reply