lpc link compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc link compatibility

690 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by multivac on Fri May 21 19:12:12 MST 2010
hi!
i was wondering if the separated LPClink and IDE can be used as a debugger for any jtag compatible device(e.g. LPC2103), or if it will only work with those specified in the LPCXpresso homepage?
thanks in advance
0 Kudos
Reply
1 Reply

676 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri May 21 23:21:44 MST 2010
LPC-Link can be used to debug any LPC device.

However, LPCXpresso only supports a limited set of devices. You have to upgrade to Red Suite (either one of the NXP editions, or the full edition) to get the support for other parts.

Red SUite NXP Editions starts from $256 for a 256k limited version.
0 Kudos
Reply