lpc link 2 configuration tool problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc link 2 configuration tool problem

986件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by internav on Fri Jan 02 08:05:50 MST 2015
installed link2 configuration tool and try to run.  Get error message invalid win32 Application.   This is on a XP  SP3 32 bit machine.  Does this not work on 32 bit?   NET4 is installed.
0 件の賞賛
返信
2 返答(返信)

965件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Fri Jan 02 10:10:16 MST 2015
The LCT v2.00 was built with VS2010 using NET4, while v2.01 was built with VS2013 using NET4.5. Unfortunately, it looks like an option for enabling legacy XP support was not turned on for v2.01 when the project was switched to VS2013.

We'll re-enable this support for a future release, but for now, you can use the older v2.00 LCT binary which is in the v2.00 installer.
This can still be downloaded here (direct link): http://www.lpcware.com/system/files/lct_installer.exe

It might still be a good time to consider an OS upgrade (but I can understand if you don't want to!)..
0 件の賞賛
返信

965件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri Jan 02 08:17:46 MST 2015
I would guess that NXP don't support on XP any more (seeing as it has been obsolete since April 2014). Using Visual Studio you have to specifically enable XP support in your executable and it looks like they have chosen not to.

Time to upgrade your computer and/or OS...
0 件の賞賛
返信