license error on unmodified sample

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

license error on unmodified sample

2,887 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Sat Apr 26 15:41:55 MST 2014
Hi,

Using the supplied activation key, with your example AN11121 code, as delivered,
USB CCID class smart card reader, no changes. Ran import, build, debug and I got the following license error.
See attached pdf

How can I fix it?

Thanks,
0 Kudos
Reply
8 Replies

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon May 05 09:14:41 MST 2014

Based on the data you've provided, NXP has identified a license problem processing your Linux machine configuration. This will be resolved in the next maintenance release which should be available within a week. Sorry for the inconvenience.

Regards,

LPCXpresso-Support
0 Kudos
Reply

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bilbolodz on Wed Apr 30 13:07:57 MST 2014
Information you've asked in attachment.
0 Kudos
Reply

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bilbolodz on Wed Apr 30 06:13:07 MST 2014
Ubuntu 12.04 ZIP attached

0 Kudos
Reply

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Apr 30 05:20:27 MST 2014
Which distro and version of Linux are you running?

Please zip up and post the usr/share/NXPLPCXpresso directory.
0 Kudos
Reply

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bilbolodz on Wed Apr 30 05:16:10 MST 2014
Still the same. I've removed old (7.0.2) and installed new versiosn (7.1.1). I've also made "a new registration" :

Help->Activate->Create serial
Help->Activate->Activate

License type: FULL
Debug limit: 256k
Activation code: removed

bilbo@pc-bilbo:/usr/local/lpcxpresso_7.1.1_125/lpcxpresso/bin$ ./crt_emu_cm3_nxp -info-license
Ni: LPCXpresso Debug Driver v7.0 (Mar 26 2014 18:35:04 - crt_emu_cm3_nxp build 1243)
Cr:f PCXpresso Free License - Download limit is 8K (UNREGISTERED)
0 Kudos
Reply

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Apr 30 04:28:39 MST 2014
If you activated the product, then you will not have needed to create the Symlink.

Please delete the symlink and activate the product as specified in the User Manual.

Note: If you used a version of LPCXpresso prior to v6, you MUST reactivate.

BTW: the vbscript comments are for Windows only.
0 Kudos
Reply

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bilbolodz on Wed Apr 30 04:08:11 MST 2014
I've same problem as [email protected] (on linux). I've read FAQ about "image too large" but I don't quite understand how should I test vbs scripting under linux. I've tried to test "All platforms" solution and got:

bilbo@pc-bilbo:~/tmp$ /usr/local/lpcxpresso_7.0.2_102/lpcxpresso/bin/crt_emu_cm3_nxp -info-license
Ni: LPCXpresso Debug Driver v6.0 (Mar  7 2014 05:14:33 - crt_emu_cm3_nxp build 1230)
Cr:f PCXpresso Free License - Download limit is 8K (UNREGISTERED)

I didn't found /usr/share/LPCXpresso directory on my system but found /usr/share/LPCXpresso with contents:

bilbo@pc-bilbo:~/tmp$ ls -l /usr/share/NXPLPCXpresso/
razem 8
-rw-rw-rw- 1 bilbo bilbo  64 kwi 30 12:10 LPCXpresso.acc
-rw-rw-rw- 1 bilbo bilbo 296 kwi 30 12:08 LPCXpresso.sib

so I've made a symlink

bilbo@pc-bilbo:~/tmp$ ls -l /usr/share/LPCXpresso
lrwxrwxrwx 1 root root 25 kwi 30 12:58 /usr/share/LPCXpresso -> /usr/share/NXPLPCXpresso/

but it doesn't fix problem.

In log I'm only found:

!ENTRY com.crt.dsfdebug 4 0 2014-04-30 12:32:15.168
!MESSAGE License restriction: Flash image too large for this license.
0 Kudos
Reply

2,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat Apr 26 15:53:54 MST 2014
Did you try License diagnostics already?

http://www.lpcware.com/content/faq/lpcxpresso/flash-image-too-large

0 Kudos
Reply