licence restriction?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

licence restriction?

834件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by janek on Wed Jul 28 20:43:02 MST 2010
Hi,
I am trying to program the latest 'usbcdc' project into my LPCXPRESSO board based on LPC1343F but have no luck.
I started with 'blinky' project and it works.
The error in popup window is:
"Error reported by target
Target reported errors
Reason:
Licence restriction:Flash image too large for this licence"
What is the problem and how to fix it.
I have two boards with the same error.
Jan
[LEFT][SIZE=1]LPCXpresso: [/SIZE][/LEFT]
[SIZE=1]Build id: LPCXpresso v3.4.0 [Build 187] [23/06/2010] [/SIZE]
0 件の賞賛
返信
2 返答(返信)

825件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by janek on Thu Jul 29 04:18:37 MST 2010
Hi,
By requesting and installing another activation code the problem dissappered.
Thank you.
Jan
0 件の賞賛
返信

825件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jul 28 23:48:33 MST 2010
It looks like yu have a license issue.
Please open a command window in <install>/bin directory and run
crt_emu_lpc11_13_nxp -info-license

Then, depending on your OS, zip and post send the "LPCXpresso" directory:
(XP) C:\Documents and Settings\All Users\LPCXpresso
(Vista/Win7) C:\Users\Public\LPCXpresso
0 件の賞賛
返信