launch configuration is incompatible

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

launch configuration is incompatible

2,778件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Wed Jan 21 05:47:29 MST 2015
I have installed new lpcxpresso version 7.5 and i have this error when try to enter in debug mode

Incompatible launch configuration
  The launch configuration (xxxxxxx Release) is incompatible with this version of LPCXpresso.
  Please delete and recreate the launch configuration.

What can i do to solve it ?
0 件の賞賛
返信
10 返答(返信)

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 25 07:00:00 MST 2015
Or what you could have done is just click on the Debug option in the Quickstart panel. Then your launch configuration would have been automatically created.

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gslomin on Thu Sep 24 15:58:02 MST 2015
In order for LPCXpresso to recreate my launch configurations I had to right click on my project Run As->C/C++ MCU Application

After this I was presented with a screen asking which .axf file to use for the launch (Debug or Release)
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jan 21 08:53:39 MST 2015
As I said before, you just need to delete the Launch configuration. To do this, either
- right-click on the Project, Select Launch Configuration and then Delete, or
- right-click on the Project, Select Launch Configiration and then Edit current. And in the Dialog show, delete the configuration from the list on the right, or
- delete the *.launch files in your project

If you are getting the same error, you did not delete it...
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Wed Jan 21 08:30:32 MST 2015

Quote: R2D2

Quote: blasiis
Sorry, but after delete the .launch with progect menu, the clean and build all don't create it and remain the same error



Try to import it...



What's import ? project ?
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jan 21 07:47:22 MST 2015

Quote: blasiis
Sorry, but after delete the .launch with progect menu, the clean and build all don't create it and remain the same error



Try to import it...
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Wed Jan 21 07:40:01 MST 2015
Sorry, but after delete the .launch with progect menu, the clean and build all don't create it and remain the same error
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jan 21 07:14:26 MST 2015

Quote: blasiis
Ok, how can I delete and recreate it ?



Select *.launch files of your project (in Project Explorer) and delete them...

LPCXpresso will create new (hopefully working) ones again, if you build the project again  :)
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jan 21 07:07:36 MST 2015
http://www.lpcware.com/content/faq/lpcxpresso/launch-configuration-menu
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Wed Jan 21 07:05:27 MST 2015
Ok, how can I delete and recreate it ?
0 件の賞賛
返信

2,632件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jan 21 06:06:07 MST 2015

Quote: blasiis
What can i do to solve it ?



:quest:



Quote:
Please delete and recreate the launch configuration.



Just delete your launch configuration as requested...
0 件の賞賛
返信