jre error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

jre error

1,625件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by renan on Mon Sep 20 16:20:38 MST 2010
When I try to run LPCXpresso for linux, I got this error:

$ ./lpcxpresso
#
# A fatal error has been detected by the Java Runtime Environment:
#
#  SIGSEGV (0xb) at pc=0xb271cc42, pid=4614, tid=3076785856
#
# JRE version: 6.0_18-b07
# Java VM: Java HotSpot(TM) Client VM (16.0-b13 mixed mode, sharing linux-x86 )
# Problematic frame:
# C  [libxul.so+0x99ec42]
#
# An error report file with more information is saved as:
# /tmp/hs_err_pid4614.log
#
# If you would like to submit a bug report, please visit:
#   http://java.sun.com/webapps/bugreport/crash.jsp
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
Aborted

The log file is attached.

Thanks,
Renan
0 件の賞賛
返信
6 返答(返信)

1,613件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gordonwall on Thu Apr 28 15:51:01 MST 2011
As you may notice, problem is connected with libxul.so which is part of xulrunner package. Downgrading to xulrunner-1.9.2.9 fixed this in my case.
0 件の賞賛
返信

1,613件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Sep 21 05:06:24 MST 2010
The one we supply...

Sun JRE version: 6.0_18-b07
0 件の賞賛
返信

1,613件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by renan on Tue Sep 21 04:17:38 MST 2010
What is the version of the JRE you recommend?

Renan
0 件の賞賛
返信

1,613件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Sep 21 04:04:04 MST 2010
This is the standard Sun JRE, so there must be a problem with the distro you are using. Suggest you ask whoever supports your distro to ask why the Sun JRE doesn't work.
0 件の賞賛
返信

1,613件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by renan on Tue Sep 21 03:56:29 MST 2010
No, it is not one of the supported distros, it is Chakra, based on Arch Linux.
What caused that error?

Renan
0 件の賞賛
返信

1,613件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Sep 20 23:17:59 MST 2010
I see from the log that this is Linux. Which distro is it? As far as I can tell, it is not one of the supported distros.
0 件の賞賛
返信