how to program off-chip memory without using on-chip memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to program off-chip memory without using on-chip memory

412件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SHEKAR MJ on Wed May 28 06:41:51 MST 2014
I m using lpc1777 controller which is having 512kb on-chip flash but my code is exceeding this memory(becoz of some cg array i used) so i m using external flash of 2MB when I programmed this through JTAG it is programmed again I tried to program it is showing cannot access memory. Is there any conflict b/w code on on-chip and code on external flash. And now I replaced the controller with new one it is working fine in on-chip mode so is there any configuration to do for not to use on-chip memory.
0 件の賞賛
返信
0 返答(返信)