frequency of the peripheral I²C clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frequency of the peripheral I²C clock

425 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wama on Tue Mar 06 06:40:37 MST 2012
I'm using LPC1114 running at 24Mhz.

At the moment I'm trying to send data over I²C. To calculate the I²C bit frequency I need to know the frequency of the peripheral I²C clock.
Is this the same value than my main clock?
0 Kudos
Reply
1 Reply

413 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Carrigan on Tue Mar 06 07:24:07 MST 2012
Page 14 of the LPC1114 User manual has a great picture of the clock setup of this device. You can see here that the "System Clock" coming out of the SYSAHBCLKDIV block is tied to both the Cortex-M0 processor as well as the AHBCLKCTRL control register. Since there is not an individual clock for the I2C like there is for SPI and UART, this means that the clock coming in to the I2C module is the same as the system clock.

Note that you will have to divide this clock using the SCLH and SCLL registers to bring it down to acceptable values (pg 166). The maximum frequency that the 1114 supports is 1MHz in Fast-mode Plus.
0 Kudos
Reply