flash tool for LPC link without LPCXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash tool for LPC link without LPCXpresso IDE

701件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hoellencrosser on Thu Nov 08 06:01:12 MST 2012
Hello

I am searching for a small tool to programm a LPC1114 with the LPC-Link. Unfortunatly I used the UART pins on my custom board for different function so I cannot use the UART-bootloader of the chip. The Flash tool from NXP inside the CodeRed IDE is nice but many users do want to install this big IDE. Is it possible to extract the flash tool so that users can just start the flash tool and program the chip with the LPC-Link?
0 件の賞賛
返信
1 返信

669件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Macgyver on Thu Nov 08 15:07:43 MST 2012
I have also wondered this and have been searching for a solution.
0 件の賞賛
返信