fedora19 lpcxpresso error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fedora19 lpcxpresso error

1,160 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattes on Tue Jan 28 10:01:23 MST 2014
just tried to run the lpcxpresso on Fedora 19.

$ /usr/local/lpcxpresso_6.1.4_194/lpcxpresso/lpcxpresso
#
# A fatal error has been detected by the Java Runtime Environment:
#
#  SIGSEGV (0xb) at pc=0x4596b1be, pid=1706, tid=3077756608
#
# JRE version: 7.0_25-b30
# Java VM: OpenJDK Client VM (23.7-b01 mixed mode linux-x86 )
# Problematic frame:
# C  [libsoup-2.4.so.1+0x561be]  soup_session_feature_detach+0x1e
#
# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again
#
# An error report file with more information is saved as:
# /home/mattes/hs_err_pid1706.log
#
# If you would like to submit a bug report, please include
# instructions on how to reproduce the bug and visit:
#   https://bugs.launchpad.net/ubuntu/+source/openjdk-7/
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
Aborted (core dumped)

I updated Fedora 19 to the latest (yum update) and it still behaves the same way.

Installed lpcxpresson from scratch.
On start it comes up with the initial lpcxpresso screen and sets up the working directory and
then it folds.

it crashes with a libsoup error

is there a fix available for this?
Does any other lpcxpresson version to work under Fedora 19?

mat

Original Attachment has been moved to: hs_err_pid1706.log_.txt.zip

0 项奖励
回复
5 回复数

1,096 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattes on Tue Jan 28 22:45:19 MST 2014

Quote: lpcxpresso-support
Please add the suggested changes to LPCXpresso.ini and not eclipse.ini.



thank you. Now it starts up and I was able to register it
0 项奖励
回复

1,096 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jan 28 15:09:29 MST 2014
Please add the suggested changes to LPCXpresso.ini and not eclipse.ini.
0 项奖励
回复

1,096 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattes on Tue Jan 28 13:54:14 MST 2014

Quote: lpcxpresso-support
This is a problem in Eclipse. You can read about it and possible workarounds at
https://bugs.eclipse.org/bugs/show_bug.cgi?id=404776

(Comment #22 seems to provide a usable workaround).



I added the following to eclipse.ini:

  -Dorg.eclipse.swt.browser.DefaultType=mozilla
  -Dorg.eclipse.swt.browser.XULRunnerPath=/usr/lib/xulrunner

But no change. It is still crashing.  I cannot even get to license it.

Is the fix dependant on what version of mozilla/xulrunner is installed?

On Fedora 19 with the latest update the following is available:
  rpm -q firefox xulrunner eclipse-platform
  firefox-26.0-2.fc19.i686
  xulrunner-26.0-1.fc19.i686
  eclipse-platform-4.3.1-5.fc19.i686

According to the bug report it was supposed to be fix with eclipse-4.3. but it seems not.

Any other workaround available?
Is there a way to configure lpcxpresso to not exercise the steps that make it crash?

Mat
0 项奖励
回复

1,096 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jan 28 10:43:01 MST 2014
This is a problem in Eclipse. You can read about it and possible workarounds at
https://bugs.eclipse.org/bugs/show_bug.cgi?id=404776

(Comment #22 seems to provide a usable workaround).
0 项奖励
回复

1,096 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattes on Tue Jan 28 10:40:26 MST 2014
installed LPCXpresso v5.2.6 which fails in the same way (libsoup error) as v6 does
installed  LPCXpresso v4.3.0 which actually starts up after installation and i was able to activate it.

0 项奖励
回复