does LPC Xpresso supports development on using LPC2129

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does LPC Xpresso supports development on using LPC2129

1,423 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by suhel on Mon Oct 20 08:41:48 MST 2014
Hi,

I want to use LPC2129 for my project and wanted to know if i can use LPC xpresso for software development.

Please do reply.

Also, are there any development boards available which can be readily used for development.

Regards,
Suhel
0 Kudos
Reply
5 Replies

1,385 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by graynomad on Wed Oct 22 08:49:41 MST 2014

Quote:
I choose 2129 only because of the easy availability of the development boards.


You can't get easier availability than the current range of Xpresso boards.

I am a recent fan boy of the 15xx series and would recommend looking at them.
0 Kudos
Reply

1,385 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Tue Oct 21 06:17:29 MST 2014

Quote: suhel
...
I am working on CAN, i know this peripheral is available on many other newer parts.

I choose 2129 only because of the easy availability of the development boards.

Please share your thoughts.



I would recommend to use a M3. The best option would be a LPC15xx. It's including 1 CAN channel and CAN bootloader. EEPROM, SWM and modern timers are very useful...

It's available in LQFP48 - LQFP100, so building your own board isn't too difficult...
0 Kudos
Reply

1,385 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Oct 21 04:14:00 MST 2014
I echo the comments made by thefallguy. You really should be looking at Cortex-M based parts. These MCUs and boards for them are very widely available, with lots of example code etc.

For example, take a look at the various LPCXpresso boards, details of which can be found at:

http://www.lpcware.com/LPCXpressoBoards

Regards,
LPCXpresso Support
0 Kudos
Reply

1,385 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by suhel on Mon Oct 20 10:30:33 MST 2014
Thanks for your reply.

The project i am working on is for study purpose so, i believe i am fine to use this part.

I am working on CAN, i know this peripheral is available on many other newer parts.

I choose 2129 only because of the easy availability of the development boards.

Please share your thoughts.

Regards,
Suhel
0 Kudos
Reply

1,385 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Oct 20 08:51:34 MST 2014
Before starting on development using an old part like this, suggest you take a look at this:
http://www.nxp.com/techzones/microcontrollers-techzone/longevity.html

This says the 2129 'longevity' date is 2017-08 - i.e. less than 3 years away...

You might want to consider one of the newer Cortex-M0 or Cortex-M3 parts, depending on your requirements.
0 Kudos
Reply