cmsis and lpc11u35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cmsis and lpc11u35

717 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ronkrem on Wed Aug 22 03:51:20 MST 2012
I have purchased the Embedded Artists LPC11U35 quickstart board and quickly got its blinky project going. However, now I want to move an existing lpc1114 project across to the '35 and this includes drivers for counters, usart, spi, etc. None of the sample expresso projects seem to include the '35, and I am wondering if anyone on this list has some clues on how to begin building a complex project with the '35.

Cheers, Ron
0 Kudos
Reply
1 Reply

710 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by graynomad on Thu Aug 23 06:09:32 MST 2012
I just got into the LPCs and have started with the 1227, there are not many examples for that either so I've just had to plug away by myself. Also most of the examples I find on the web appear to be for non-GCC toolchains because they invariably never even compile.

In the case of the 1227 (and any other Xpresso CPU) you can buy a base board and that gives you access to more examples. This I have done although I haven't used the new code yet. That's not much help to you though I guess.

If you have working 1114 CMSIS code surely it will port across without too much work.
0 Kudos
Reply