c_type librarybeing compiled in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

c_type librarybeing compiled in

916件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andy on Thu Feb 03 23:21:55 MST 2011
I have a project which compiles and runs using lpcxpresso under linux (version 3.8.2) which does not compile in the c_type library. so I can reasonably assume it is not needed,  but under windows (version 3.5.0 and 3.6.2)  it does using an additional 824bytes of flash.

is this due to the different versions of gcc and can I add a another compiler option to fix this ?
0 件の賞賛
返信
2 返答(返信)

894件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdseymour on Fri Feb 11 18:04:43 MST 2011
I'm struggling with this same issue. Does anyone know of a workaround to keep the ctype module from being linked in?
0 件の賞賛
返信

894件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Feb 04 00:24:52 MST 2011
The Linux version of LPCXpresso uses an updated version of Redlib compared to the Windows version, which provides some code and data size saving from a number of internal changes - including the ctype one that you note.

There is some more information on the new "Redlib_v2" at:

http://support.code-red-tech.com/CodeRedWiki/redlib_v2_notes

We are working at bringing the two versions into line in a forthcoming  new version of the tools. However I can't make any comment at present as  to when this will be released.

Regards,
CodeRedSupport
0 件の賞賛
返信