adding extern include folder to project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adding extern include folder to project

1,228 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by justmakeit on Fri Jan 29 01:39:34 MST 2016
Currently i copy a whole project folder to create a new project. But its a lot of work to update all older projects to the current software versions. There must be a better way to do this.
maybe there is a way to add a shared folder outside the workspace to my projects. but i cant add a source folder outside my workspace to my project in lpcxpresso. What is the right work flow to use?
I hope my question is clear enough...

Thank you in advance
0 Kudos
Reply
3 Replies

1,217 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by justmakeit on Fri Jan 29 03:01:50 MST 2016
can i include files from my workspace to a library? like a config.h for every project. or is a library pre compiled?
0 Kudos
Reply

1,217 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Fri Jan 29 02:09:38 MST 2016
As well as trying a library, you can also use "Linked folders". This is described in the docs
0 Kudos
Reply

1,217 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Jan 29 01:59:01 MST 2016

Quote: justmakeit
What is the right work flow to use?



What's wrong with using a library?
0 Kudos
Reply