Windows error message when starting debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Windows error message when starting debug

634 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thanseen on Mon Jan 24 15:33:23 MST 2011
I'm new to LPCXpresso and the Eclipse IDE.  Just unpacked my board today.  Every time I start a debug session, this Windows error comes up:

"crt_emu_cm3_nxp.exe has encountered a problem and needs to close..."

The debug session seems to work OK, but getting the error every time bothers me.  Is this a bug in the IDE or am I doing something wrong?

Thanks!
0 项奖励
回复
1 回复

625 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jan 25 01:43:26 MST 2011
This is a little curious. In the first place can you provide a bit more information on your setup...

[LIST]
[*]What operating system are you using? And are you running it natively or via a virtual machine.
[*]What version of the LPCXpresso IDE are you using?
[*]Which LPCXpresso board are you connecting to?
[*]Are you connecting the LPCXPresso board directly to your PC's USB   port, or via a USB hub. If via a hub, then try connecting directly. If   directly, try via a powered hub (we don't normally recommend the use of a   hub, but if you have a power issue with the USB ports on your PC, then   this might help.
[*]Do you have any other hardware connected the the LPCXPresso board   (external hardware, including, for example, an Embedded Artists   baseboard). If so, try removing it.
[/LIST]
One possibility that might be causing this is the use of "cscript". It might be worth you have a look at previous threads regarding this and see if anything in these gives you any clues when mapped onto the PC in front of you. Do a google search using "cscript site:knowledgebase.nxp.com" to find these.

Regards,
CodeRedSupport.
0 项奖励
回复