Windows 7 64 bit DFU driver - any progress?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 7 64 bit DFU driver - any progress?

2,005 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brucesegal on Tue Feb 23 09:40:29 MST 2010
I know that this has been discussed before, but is there any idea when/if 654 bit drivers will be available for the DFU portion of the LPC Link?

The workaround (XP mode) is ungainly and it seems relatively trivial to recompile the driver for 64 bit.

Thanks,
0 Kudos
Reply
7 Replies

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by termohlen on Tue Mar 09 20:06:20 MST 2010
I neither have Windows 7 x64 Pro nor do I have the hardware to support virtuallization... also, I am participating in the challenge.  I will have to run from a 2003 vintage laptop  :(
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brucesegal on Thu Mar 04 21:27:47 MST 2010

Quote: NXP_USA
Stay tuned. We may be looking for beta testers within a few weeks.

-NXP



Be still my beating heart! Great news.
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Mar 04 14:19:20 MST 2010

Quote: brucesegal
Thanks for the update.

Bruce



Stay tuned. We may be looking for beta testers within a few weeks.

-NXP
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brucesegal on Sun Feb 28 14:08:17 MST 2010
Thanks for the update.

Bruce
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Sun Feb 28 00:16:44 MST 2010

Quote: Rob65
Good question.
This one pops up now and then but the only answer I have seen up to now is that "we are working on it". It seems a bit strange that with the current move from 32 to 64 bit operating systems a DFU driver for these devices is not available.

It would be great if NXP could tell us what the expected delivery date of the driver is.

Rob



LPCXpresso with 64-bit Windows Vista/Windows 7 support should be available within the next few months. We apologize for not having an exact date at this time.

-NXP
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tkreyche on Thu Feb 25 21:01:24 MST 2010
64-bit drivers are a no brainer - any higher end laptop you buy now will be 64 bit. And it's any easy compile option to create them, assuming the source code is reasonably standard.
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Thu Feb 25 11:32:56 MST 2010
Good question.
This one pops up now and then but the only answer I have seen up to now is that "we are working on it". It seems a bit strange that with the current move from 32 to 64 bit operating systems a DFU driver for these devices is not available.

It would be great if NXP could tell us what the expected delivery date of the driver is.

Rob
0 Kudos
Reply