Weirdness in UARTs during debug session

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Weirdness in UARTs during debug session

1,056件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JGold on Thu Sep 23 06:49:12 MST 2010
When I am running the debugger, and look at the peripheral window for UART2, I get incorrect feedback.  See the attached clip.  The register UDLM at address 0x40098004 has bits listed under it for the modem signals for UART1 U1MSR register.  Also, UART2 UDLL does not report correctly for the baudrate I am running.  Lastly, UART3 is being used, but is being shown as disabled.[ATTACH]192[/ATTACH]
0 件の賞賛
返信
3 返答(返信)

1,050件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 23 08:23:28 MST 2010
This has now been fixed and will be in the next release of LPCXpresso.

Thanks for reporting it.
0 件の賞賛
返信

1,050件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JGold on Thu Sep 23 07:11:07 MST 2010
Lpc1765
0 件の賞賛
返信

1,050件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 23 07:10:00 MST 2010
Hi,

Can you tell us which part you are using?
0 件の賞賛
返信