Wakeup as ADC trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wakeup as ADC trigger

420 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ruchika123 on Mon Feb 22 21:51:54 MST 2016
Hi,

I am using the LPCXpresso board with LPC1549. I have got a wakeup switch on the board which i want to use as the hardware trigger for the ADC but when i assign PINTRIG0 or PINTRIG1 to the pin connected to the wakeup button on the board which is PO0_17, i cannot use it as a trigger. For testing that pin as the trigger i toggle the onboard LED to test its triggering but the LED does not toggle. I cannot get any detailed information wheather PO0_17 can be used as an external trigger or not. I need help on this.



Thanks,
Ruchika
0 Kudos
Reply
0 Replies