WHIS Stateviewer not working.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

WHIS Stateviewer not working.

738 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chris_bayley_trimble on Sun Nov 02 18:52:22 MST 2014
Hi all,

I'm running LPCXpresso v7.4.0 [Build 229] on OSX 10.9.3 with WHIS StateViewer2.0.8.201409041322 installed.
The FreeRTOS version under test is 8.0.1
I'm using an LPC Link 2 with the standard firmware (Redlink or what have you)

I'm not getting any info into any of the state viewer windows (Queues,Tasks,Timers) using either the DSF views or the legacy style.

I've read through the install and usage docs many time and can't identify anything I might have missed. Is anyone aware of the 'workingness' of my combination of versions or any problems therewith ?
Is there anything I can do to locate the problem or is it an issue to raise with WHIS ?

Cheers all,
Chris
0 项奖励
回复
1 回复

689 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Nov 02 20:00:37 MST 2014
You will need to contact WHIS. Tell them that you are using LPCXpresso v7.4 (which is based on Eclipse 4.4 'Luna' and CDT 8.4).
0 项奖励
回复