WHIS Stateviewer not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WHIS Stateviewer not working.

739 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chris_bayley_trimble on Sun Nov 02 18:52:22 MST 2014
Hi all,

I'm running LPCXpresso v7.4.0 [Build 229] on OSX 10.9.3 with WHIS StateViewer2.0.8.201409041322 installed.
The FreeRTOS version under test is 8.0.1
I'm using an LPC Link 2 with the standard firmware (Redlink or what have you)

I'm not getting any info into any of the state viewer windows (Queues,Tasks,Timers) using either the DSF views or the legacy style.

I've read through the install and usage docs many time and can't identify anything I might have missed. Is anyone aware of the 'workingness' of my combination of versions or any problems therewith ?
Is there anything I can do to locate the problem or is it an issue to raise with WHIS ?

Cheers all,
Chris
0 Kudos
Reply
1 Reply

690 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Nov 02 20:00:37 MST 2014
You will need to contact WHIS. Tell them that you are using LPCXpresso v7.4 (which is based on Eclipse 4.4 'Luna' and CDT 8.4).
0 Kudos
Reply