Using intertnal bootloader via Bluetooth module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using intertnal bootloader via Bluetooth module

893 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by celephicus on Mon Nov 19 22:07:31 MST 2012
We are using a Roving Networks Bluetooth module & a LPC1113 in a product, and it occurs to me that I could upload the code using the bootloader  via the Bluetooth link, since it can be setup to look like a virtual COM port on the PC end, and just spits out 8N1 serial data at 115200 baud at the LPC1113 end.

Has anyone tried this?
0 项奖励
回复
1 回复

886 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fjrg76 on Tue Nov 20 19:58:27 MST 2012
Not yet, but ... besides the Tx and Rx pins, you need to control the ISP and reset pins too. If so, it's pretty shure you can achieve your goal.
0 项奖励
回复