Using Timer INT without Hardware Pin-Out MATx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using Timer INT without Hardware Pin-Out MATx

704件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by StephenHawkings on Mon Sep 12 02:34:49 MST 2011
Dear Collegues,
would wou agree that it's possible to use the timer INTs without changing the corresponding I/O pins (MATx and CAPx)? I just want to use the timer interrupts internal, but keep the I/O pins as simple I/Os. (I use LPC1114, but probably behaviour is the same across all LPCs.)

Thank you for your comments!
StephenHawkings
0 件の賞賛
返信
1 返信

697件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Sep 12 02:38:08 MST 2011
In general....yes :)
0 件の賞賛
返信